InheritPmiViewStyle Class¶
-
class
NXOpen.Drawings.
InheritPmiViewStyle
¶ Bases:
object
Represents set of InheritPmiViewStyle applicable to drafting views.
To obtain an instance of this class use
Drawings.ViewStyle.InheritPmi()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
CrosshatchPmiLwsv | Returns the cross-hatch setting for the current inherited PMI Lightweight Section View |
InheritPmiMode | Returns or sets the Inherit pmi mode. |
InheritPmiToDrawing | Returns or sets the status of pmi inherited to drawing. |
InheritPmiTypeMask | Returns or sets the Inherit pmi type mask. |
PmiDimensionFromRevolved | Returns or sets the status of pmi inherited to drawing. |
Methods¶
Method | Description |
---|---|
SetCrosshatchPmiLwsv | Controls whether the cut faces of an inherited PMI Lightweight section view are cross-hatched or not. |
SetInheritGdt | Inherit GD and T option,that let you inherit GD and T display instances onto the drawing plane or into a drawing member view. |
Property Detail¶
CrosshatchPmiLwsv¶
-
InheritPmiViewStyle.
CrosshatchPmiLwsv
¶ Returns the cross-hatch setting for the current inherited PMI Lightweight Section View
-------------------------------------
Getter Method
Signature
CrosshatchPmiLwsv()
Returns: the crosshatch flag setting Return type: bool New in version NX8.0.0.
License requirements: None.
InheritPmiMode¶
-
InheritPmiViewStyle.
InheritPmiMode
¶ Returns or sets the Inherit pmi mode.
-------------------------------------
Getter Method
Signature
InheritPmiMode()
Returns: Return type: NXOpen.Preferences.PmiOption
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InheritPmiMode(pmiOption)
Parameters: pmiOption ( NXOpen.Preferences.PmiOption
) –New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
InheritPmiToDrawing¶
-
InheritPmiViewStyle.
InheritPmiToDrawing
¶ Returns or sets the status of pmi inherited to drawing.
-------------------------------------
Getter Method
Signature
InheritPmiToDrawing()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InheritPmiToDrawing(pmiToDrawing)
Parameters: pmiToDrawing (bool) – New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
InheritPmiTypeMask¶
-
InheritPmiViewStyle.
InheritPmiTypeMask
¶ Returns or sets the Inherit pmi type mask.
-------------------------------------
Getter Method
Signature
InheritPmiTypeMask()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InheritPmiTypeMask(pmiTypeMask)
Parameters: pmiTypeMask (int) – New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
PmiDimensionFromRevolved¶
-
InheritPmiViewStyle.
PmiDimensionFromRevolved
¶ Returns or sets the status of pmi inherited to drawing.
-------------------------------------
Getter Method
Signature
PmiDimensionFromRevolved()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PmiDimensionFromRevolved(pmiDimensionFromRevolved)
Parameters: pmiDimensionFromRevolved (bool) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
SetCrosshatchPmiLwsv¶
-
InheritPmiViewStyle.
SetCrosshatchPmiLwsv
¶ Controls whether the cut faces of an inherited PMI Lightweight section view are cross-hatched or not.
Signature
SetCrosshatchPmiLwsv(crosshatch)
Parameters: crosshatch (bool) – New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
SetInheritGdt¶
-
InheritPmiViewStyle.
SetInheritGdt
¶ Inherit GD and T option,that let you inherit GD and T display instances onto the drawing plane or into a drawing member view.
Signature
SetInheritGdt(gdtOption)
Parameters: gdtOption ( NXOpen.Preferences.GdtOption
) – Inherit GDT optionNew in version NX5.0.0.
License requirements: drafting (“DRAFTING”)