SectionLineStyleBuilderArrowheadStyleType Enumeration¶
NXOpen.Drawings.SectionLineStyleBuilder.ArrowheadStyleType is an alias for NXOpen.Drawings.SectionLineStyleBuilderArrowheadStyleType
-
class
NXOpen.Drawings.
SectionLineStyleBuilderArrowheadStyleType
¶ Bases:
object
This enum represents arrowhead style type.
Deprecated since version NX10.0.0: Use
NXOpen.Drawings.ViewSectionLineBuilder.StyleType()
instead.Enum Members
Enum Member Enum Member Description Open Closed Filled -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-