ViewAlignmentCollection Class

class NXOpen.Drawings.ViewAlignmentCollection

Bases: object

Represents a collection of :py:class:`NXOpen.Drawings.ViewAlignment`s.

To obtain an instance of this class, refer to NXOpen.Part

New in version NX8.5.0.

Methods

Method Description
CreateViewAlignmentBuilder Creates a NXOpen.Drawings.ViewAlignmentBuilder @return
FindObject Finds the NXOpen.Drawings.ViewAlignment with the given identifier as recorded in a journal.

Method Detail

CreateViewAlignmentBuilder

ViewAlignmentCollection.CreateViewAlignmentBuilder

Creates a NXOpen.Drawings.ViewAlignmentBuilder

Signature CreateViewAlignmentBuilder()

Returns:
Return type:NXOpen.Drawings.ViewAlignmentBuilder

New in version NX8.5.0.

License requirements: drafting (“DRAFTING”)

FindObject

ViewAlignmentCollection.FindObject

Finds the NXOpen.Drawings.ViewAlignment with the given identifier as recorded in a journal.

An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.

An exception will be thrown if no object can be found with the given journal identifier.

Signature FindObject(journalIdentifier)

Parameters:journalIdentifier (str) – Identifier of the view alignment to be found
Returns:View alignment with this identifier
Return type:NXOpen.Drawings.ViewAlignment

New in version NX8.5.0.

License requirements: None.