ViewStyleSectionBuilder Class

class NXOpen.Drawings.ViewStyleSectionBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents the SECTION tab on the View Style Dialog (Drawings.

ViewStyleSectionBuilder)

New in version NX6.0.0.

Properties

Property Description
AdjacencyToleranceData Returns or sets the adjacency tolerance on the SECTION tab of the View Style Dialog
AssemblyTolerance Returns or sets the assembly tolerance toggle on the SECTION tab of the View Style Dialog
Background Returns or sets the background toggle on the SECTION tab of the View Style Dialog
Bendlines Returns or sets the bendlines toggle on the SECTION tab of the View Style Dialog
Crosshatch Returns or sets the crosshatch toggle on the SECTION tab of the View Style Dialog
DisplaySectionLine Returns or sets the display section line toggle on the SECTION tab of the View Style Dialog
Foreground Returns or sets the foreground toggle on the SECTION tab of the View Style Dialog
HiddenLineHatching Returns or sets the hidden line hatching toggle on the SECTION tab of the View Style Dialog
RestrictCrosshatchAngle Returns or sets the restrict crosshatch angle toggle on the SECTION tab of the View Style Dialog
SheetBodies Returns or sets the sheet bodies toggle on the SECTION tab of the View Style Dialog
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

AdjacencyToleranceData

ViewStyleSectionBuilder.AdjacencyToleranceData

Returns or sets the adjacency tolerance on the SECTION tab of the View Style Dialog

-------------------------------------

Getter Method

Signature AdjacencyToleranceData()

Returns:Returns the assembly tolerance that is on the section sub-builder
Return type:float

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature AdjacencyToleranceData(adjacencyToleranceData)

Parameters:adjacencyToleranceData (float) – Sets a new assembly tolerance on the section sub-builder

New in version NX6.0.0.

License requirements: drafting (“DRAFTING”)

AssemblyTolerance

ViewStyleSectionBuilder.AssemblyTolerance

Returns or sets the assembly tolerance toggle on the SECTION tab of the View Style Dialog

-------------------------------------

Getter Method

Signature AssemblyTolerance()

Returns:Returns the assembly tolerance toggle value that is on the section sub-builder
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature AssemblyTolerance(assemblyToleranceToggle)

Parameters:assemblyToleranceToggle (bool) – Sets a new assembly tolerance toggle value on the section sub-builder

New in version NX6.0.0.

License requirements: drafting (“DRAFTING”)

Background

ViewStyleSectionBuilder.Background

Returns or sets the background toggle on the SECTION tab of the View Style Dialog

-------------------------------------

Getter Method

Signature Background()

Returns:Returns the background toggle value that is on the section sub-builder
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Background(backgroundToggle)

Parameters:backgroundToggle (bool) – Sets a new background toggle value on the section sub-builder

New in version NX6.0.0.

License requirements: drafting (“DRAFTING”)

Bendlines

ViewStyleSectionBuilder.Bendlines

Returns or sets the bendlines toggle on the SECTION tab of the View Style Dialog

-------------------------------------

Getter Method

Signature Bendlines()

Returns:Returns the bendlines toggle value that is on the section sub-builder
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Bendlines(bendlinesToggle)

Parameters:bendlinesToggle (bool) – Sets a new bendlines toggle value on the section sub-builder

New in version NX6.0.0.

License requirements: drafting (“DRAFTING”)

Crosshatch

ViewStyleSectionBuilder.Crosshatch

Returns or sets the crosshatch toggle on the SECTION tab of the View Style Dialog

-------------------------------------

Getter Method

Signature Crosshatch()

Returns:Returns the crosshatch toggle value that is on the section sub-builder
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Crosshatch(crosshatchToggle)

Parameters:crosshatchToggle (bool) – Sets a new crosshatch toggle value on the section sub-builder

New in version NX6.0.0.

License requirements: drafting (“DRAFTING”)

DisplaySectionLine

ViewStyleSectionBuilder.DisplaySectionLine

Returns or sets the display section line toggle on the SECTION tab of the View Style Dialog

-------------------------------------

Getter Method

Signature DisplaySectionLine()

Returns:Returns the display section line toggle value that is on the section sub-builder
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DisplaySectionLine(displaySectionLine)

Parameters:displaySectionLine (bool) – Sets a new display section line toggle value on the section sub-builder

New in version NX6.0.0.

License requirements: drafting (“DRAFTING”)

Foreground

ViewStyleSectionBuilder.Foreground

Returns or sets the foreground toggle on the SECTION tab of the View Style Dialog

-------------------------------------

Getter Method

Signature Foreground()

Returns:Returns the foreground toggle value that is on the section sub-builder
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Foreground(foregroundToggle)

Parameters:foregroundToggle (bool) – Sets a new foreground toggle value on the section sub-builder

New in version NX6.0.0.

License requirements: drafting (“DRAFTING”)

HiddenLineHatching

ViewStyleSectionBuilder.HiddenLineHatching

Returns or sets the hidden line hatching toggle on the SECTION tab of the View Style Dialog

-------------------------------------

Getter Method

Signature HiddenLineHatching()

Returns:Returns the hidden line hatching toggle value that is on the section sub-builder
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature HiddenLineHatching(hiddenLineHatchingToggle)

Parameters:hiddenLineHatchingToggle (bool) – Sets a new hidden line hatching toggle value on the section sub-builder

New in version NX6.0.0.

License requirements: drafting (“DRAFTING”)

RestrictCrosshatchAngle

ViewStyleSectionBuilder.RestrictCrosshatchAngle

Returns or sets the restrict crosshatch angle toggle on the SECTION tab of the View Style Dialog

-------------------------------------

Getter Method

Signature RestrictCrosshatchAngle()

Returns:Returns the restrict crosshatch angle toggle value that is on the section sub-builder
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature RestrictCrosshatchAngle(restrictCrosshatchAngleToggle)

Parameters:restrictCrosshatchAngleToggle (bool) – Sets a new restrict crosshatch angle toggle value on the section sub-builder

New in version NX6.0.0.

License requirements: drafting (“DRAFTING”)

SheetBodies

ViewStyleSectionBuilder.SheetBodies

Returns or sets the sheet bodies toggle on the SECTION tab of the View Style Dialog

-------------------------------------

Getter Method

Signature SheetBodies()

Returns:Returns the sheet bodies toggle value that is on the section sub-builder
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SheetBodies(sheetBodiesToggle)

Parameters:sheetBodiesToggle (bool) – Sets a new sheet bodies toggle value on the section sub-builder

New in version NX6.0.0.

License requirements: drafting (“DRAFTING”)

Method Detail

Validate

ViewStyleSectionBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.