ViewCenterCoordinateBuilder Class¶
-
class
NXOpen.Drawings.
ViewCenterCoordinateBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the View center coodinate (Drawings.
ViewCenterCoordinateBuilder) .. versionadded:: NX6.0.0
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
XCoordinate | Returns or sets the X center coordinate |
XCoordinateExp | Returns the expression for the X coordinate |
YCoordinate | Returns or sets the Y center coordinate |
YCoordinateExp | Returns the expression for the Y coordinate |
ZCoordinate | Returns or sets the Z center coordinate |
ZCoordinateExp | Returns the expression for the Z coordinate |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
XCoordinate¶
-
ViewCenterCoordinateBuilder.
XCoordinate
¶ Returns or sets the X center coordinate
-------------------------------------
Getter Method
Signature
XCoordinate()
Returns: returns the center coordinate. Return type: float New in version NX6.0.0.
Deprecated since version NX7.5.0: Use
Drawings.ViewCenterCoordinateBuilder.XCoordinateExp()
License requirements: None.
-------------------------------------
Setter Method
Signature
XCoordinate(cenwcs)
Parameters: cenwcs (float) – sets the coordinate. New in version NX6.0.0.
Deprecated since version NX7.5.0: Use
Drawings.ViewCenterCoordinateBuilder.XCoordinateExp()
License requirements: nx_layout (“NX Layout”)
XCoordinateExp¶
-
ViewCenterCoordinateBuilder.
XCoordinateExp
¶ Returns the expression for the X coordinate
-------------------------------------
Getter Method
Signature
XCoordinateExp()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
YCoordinate¶
-
ViewCenterCoordinateBuilder.
YCoordinate
¶ Returns or sets the Y center coordinate
-------------------------------------
Getter Method
Signature
YCoordinate()
Returns: returns the center coordinate. Return type: float New in version NX6.0.0.
Deprecated since version NX7.5.0: Use
Drawings.ViewCenterCoordinateBuilder.YCoordinateExp()
License requirements: None.
-------------------------------------
Setter Method
Signature
YCoordinate(cenwcs)
Parameters: cenwcs (float) – sets the coordinate. New in version NX6.0.0.
Deprecated since version NX7.5.0: Use
Drawings.ViewCenterCoordinateBuilder.YCoordinateExp()
License requirements: nx_layout (“NX Layout”)
YCoordinateExp¶
-
ViewCenterCoordinateBuilder.
YCoordinateExp
¶ Returns the expression for the Y coordinate
-------------------------------------
Getter Method
Signature
YCoordinateExp()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
ZCoordinate¶
-
ViewCenterCoordinateBuilder.
ZCoordinate
¶ Returns or sets the Z center coordinate
-------------------------------------
Getter Method
Signature
ZCoordinate()
Returns: returns the center coordinate. Return type: float New in version NX6.0.1.
Deprecated since version NX7.5.0: Use
Drawings.ViewCenterCoordinateBuilder.ZCoordinateExp()
License requirements: None.
-------------------------------------
Setter Method
Signature
ZCoordinate(cenwcs)
Parameters: cenwcs (float) – sets the coordinate. New in version NX6.0.1.
Deprecated since version NX7.5.0: Use
Drawings.ViewCenterCoordinateBuilder.ZCoordinateExp()
License requirements: nx_layout (“NX Layout”)
ZCoordinateExp¶
-
ViewCenterCoordinateBuilder.
ZCoordinateExp
¶ Returns the expression for the Z coordinate
-------------------------------------
Getter Method
Signature
ZCoordinateExp()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
ViewCenterCoordinateBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.