DrawingSheetBuilderSheetBaseordrawingView Enumeration

NXOpen.Drawings.DrawingSheetBuilder.SheetBaseordrawingView is an alias for NXOpen.Drawings.DrawingSheetBuilderSheetBaseordrawingView

class NXOpen.Drawings.DrawingSheetBuilderSheetBaseordrawingView

Bases: object

the base view or drawing view option

Enum Members

Enum Member Enum Member Description
Base
auto start base view
Drawing
auto start drawing view
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.