ViewOrientationBuilder Class¶
-
class
NXOpen.Drawings.
ViewOrientationBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a ViewOrientationBuilder.
The View Orientation Block is used to specify orientation of the view, and the view being inherited or sectioned, if needed.
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
OrientationType | Returns or sets the orientation type |
SelectView | Returns the select view |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ViewOrientationBuilderOrientation Enumeration | This enum represents view orientation type. |
Property Detail¶
OrientationType¶
-
ViewOrientationBuilder.
OrientationType
¶ Returns or sets the orientation type
-------------------------------------
Getter Method
Signature
OrientationType()
Returns: Return type: NXOpen.Drawings.ViewOrientationBuilderOrientation
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientationType(orientationType)
Parameters: orientationType ( NXOpen.Drawings.ViewOrientationBuilderOrientation
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
SelectView¶
-
ViewOrientationBuilder.
SelectView
¶ Returns the select view
-------------------------------------
Getter Method
Signature
SelectView()
Returns: Return type: NXOpen.SelectView
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ViewOrientationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.