BrokenViewBuilderTypeBreak Enumeration¶
NXOpen.Drawings.BrokenViewBuilder.TypeBreak is an alias for NXOpen.Drawings.BrokenViewBuilderTypeBreak
-
class
NXOpen.Drawings.
BrokenViewBuilderTypeBreak
¶ Bases:
object
Specifies whether the break is two-sided (regular) or one-sided.
Enum Members
Enum Member Enum Member Description Regular Regular BreakSingleSided SingleSiled Break-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-