AutomationBookletBuilder Class

class NXOpen.Drawings.AutomationBookletBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.Drawings.AutomationBookletBuilder

New in version NX9.0.0.

Properties

Property Description
HiddenLineColorFontWidth Returns the hidden line color font width
Tag Returns the Tag for this object.
VisibleLineColorFontWidth Returns the visible line color font width

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

HiddenLineColorFontWidth

AutomationBookletBuilder.HiddenLineColorFontWidth

Returns the hidden line color font width

-------------------------------------

Getter Method

Signature HiddenLineColorFontWidth()

Returns:
Return type:NXOpen.LineColorFontWidthBuilder

New in version NX9.0.0.

License requirements: None.

VisibleLineColorFontWidth

AutomationBookletBuilder.VisibleLineColorFontWidth

Returns the visible line color font width

-------------------------------------

Getter Method

Signature VisibleLineColorFontWidth()

Returns:
Return type:NXOpen.LineColorFontWidthBuilder

New in version NX9.0.0.

License requirements: None.

Method Detail

Validate

AutomationBookletBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.