HingeLineBuilder Class¶
-
class
NXOpen.Drawings.
HingeLineBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a Drawings.
HingeLineBuilder. A hinge line is a line displayed on the parent view and used as a reference to rotate a child view in proper orthographic space.
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Associative | Returns or sets the infer associative setting |
ReverseDirection | Returns or sets the reverse direction setting |
SpecifyVector | Returns or sets the direction for the hinge line |
Tag | Returns the Tag for this object. |
VectorOption | Returns or sets the vector option: Inferred or Defined |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
HingeLineBuilderHingeline Enumeration | Specifies the hinge line vector option |
Property Detail¶
Associative¶
-
HingeLineBuilder.
Associative
¶ Returns or sets the infer associative setting
-------------------------------------
Getter Method
Signature
Associative()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Associative(associative)
Parameters: associative (bool) – New in version NX6.0.0.
License requirements: None.
ReverseDirection¶
-
HingeLineBuilder.
ReverseDirection
¶ Returns or sets the reverse direction setting
-------------------------------------
Getter Method
Signature
ReverseDirection()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseDirection(reverseDirection)
Parameters: reverseDirection (bool) – New in version NX6.0.0.
License requirements: None.
SpecifyVector¶
-
HingeLineBuilder.
SpecifyVector
¶ Returns or sets the direction for the hinge line
-------------------------------------
Getter Method
Signature
SpecifyVector()
Returns: Return type: NXOpen.Direction
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpecifyVector(specifyVector)
Parameters: specifyVector ( NXOpen.Direction
) –New in version NX6.0.0.
License requirements: None.
VectorOption¶
-
HingeLineBuilder.
VectorOption
¶ Returns or sets the vector option: Inferred or Defined
-------------------------------------
Getter Method
Signature
VectorOption()
Returns: The vector option Return type: NXOpen.Drawings.HingeLineBuilderHingeline
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VectorOption(vectorOption)
Parameters: vectorOption ( NXOpen.Drawings.HingeLineBuilderHingeline
) –New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
HingeLineBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.