HingeLineBuilderHingeline Enumeration

NXOpen.Drawings.HingeLineBuilder.Hingeline is an alias for NXOpen.Drawings.HingeLineBuilderHingeline

class NXOpen.Drawings.HingeLineBuilderHingeline

Bases: object

Specifies the hinge line vector option

Enum Members

Enum Member Enum Member Description
Inferred
The option to infer a hinge line based on parent, child view position
Defined
The option for selecting hinge line using vector construction tools
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.