DraftingViewCollectionViewCopyAnnotOption Enumeration

NXOpen.Drawings.DraftingViewCollection.ViewCopyAnnotOption is an alias for NXOpen.Drawings.DraftingViewCollectionViewCopyAnnotOption

class NXOpen.Drawings.DraftingViewCollectionViewCopyAnnotOption

Bases: object

Specifies the the annotation copy mode.

Enum Members

Enum Member Enum Member Description
CopyAnnotation
copy annotation
DontCopyAnnotation
don’t copy annotation
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.