BrokenViewBuilderVerticalBreakSide Enumeration¶
NXOpen.Drawings.BrokenViewBuilder.VerticalBreakSide is an alias for NXOpen.Drawings.BrokenViewBuilderVerticalBreakSide
-
class
NXOpen.Drawings.
BrokenViewBuilderVerticalBreakSide
¶ Bases:
object
Which side to remove in case of horizontal single-sided break.
Enum Members
Enum Member Enum Member Description TopEnd Hide Top sideBottomEnd Hide Bottom side-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-