ViewStyleInheritPmiBuilder Class¶
-
class
NXOpen.Drawings.
ViewStyleInheritPmiBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the INHERIT PMI tab on the View Style Dialog (Drawings.
ViewStyleInheritPmiBuilder)
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
CrosshatchPmiLwsv | Returns or sets the cross-hatch setting for the current inherited PMI Lightweight Section View |
Gdt | Returns or sets the gdt option on the INHERIT PMI tab of the View Style Dialog |
Pmi | Returns or sets the pmi option on the INHERIT PMI tab of the View Style Dialog |
PmiFromRevolved | Returns or sets the ‘Show PMI Dimensions from Revolved Sketches’ toggle on the INHERIT PMI tab of the View Style Dialog |
PmiToDrawing | Returns or sets the ‘pmi to drawing’ toggle on the INHERIT PMI tab of the View Style Dialog |
PmiTypeMask | Returns or sets the type mask on the INHERIT PMI tab of the View Style Dialog |
ReferenceSetBehavior | Returns or sets the reference set option |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CrosshatchPmiLwsv¶
-
ViewStyleInheritPmiBuilder.
CrosshatchPmiLwsv
¶ Returns or sets the cross-hatch setting for the current inherited PMI Lightweight Section View
-------------------------------------
Getter Method
Signature
CrosshatchPmiLwsv()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CrosshatchPmiLwsv(crosshatch)
Parameters: crosshatch (bool) – New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
Gdt¶
-
ViewStyleInheritPmiBuilder.
Gdt
¶ Returns or sets the gdt option on the INHERIT PMI tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Gdt()
Returns: Returns the gdt option that is on the inherit pmi sub-builder Return type: NXOpen.Preferences.GdtOption
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Gdt(gdtOption)
Parameters: gdtOption ( NXOpen.Preferences.GdtOption
) – Sets a new gdt option on the inherit pmi sub-builderNew in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Pmi¶
-
ViewStyleInheritPmiBuilder.
Pmi
¶ Returns or sets the pmi option on the INHERIT PMI tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Pmi()
Returns: Returns the pmi option that is on the inherit pmi sub-builder Return type: NXOpen.Preferences.PmiOption
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Pmi(pmiOption)
Parameters: pmiOption ( NXOpen.Preferences.PmiOption
) – Sets a new pmi option on the inherit pmi sub-builderNew in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
PmiFromRevolved¶
-
ViewStyleInheritPmiBuilder.
PmiFromRevolved
¶ Returns or sets the ‘Show PMI Dimensions from Revolved Sketches’ toggle on the INHERIT PMI tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
PmiFromRevolved()
Returns: Returns the pmi to drawing toggle value that is on the inherit pmi sub-builder Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PmiFromRevolved(pmiFromRevolvedToggle)
Parameters: pmiFromRevolvedToggle (bool) – Sets a new pmi to drawing toggle value on the inherit pmi sub-builder New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
PmiToDrawing¶
-
ViewStyleInheritPmiBuilder.
PmiToDrawing
¶ Returns or sets the ‘pmi to drawing’ toggle on the INHERIT PMI tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
PmiToDrawing()
Returns: Returns the pmi to drawing toggle value that is on the inherit pmi sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PmiToDrawing(pmiToDrawingToggle)
Parameters: pmiToDrawingToggle (bool) – Sets a new pmi to drawing toggle value on the inherit pmi sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
PmiTypeMask¶
-
ViewStyleInheritPmiBuilder.
PmiTypeMask
¶ Returns or sets the type mask on the INHERIT PMI tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
PmiTypeMask()
Returns: Returns the pmi type mask that is on the inherit pmi sub-builder Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PmiTypeMask(pmiTypeMask)
Parameters: pmiTypeMask (int) – Sets a new pmi type mask on the inherit pmi sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
ReferenceSetBehavior¶
-
ViewStyleInheritPmiBuilder.
ReferenceSetBehavior
¶ Returns or sets the reference set option
-------------------------------------
Getter Method
Signature
ReferenceSetBehavior()
Returns: Returns the pmi option that is on the inherit pmi sub-builder Return type: NXOpen.Preferences.ReferenceSetBehavior
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceSetBehavior(pmiOption)
Parameters: pmiOption ( NXOpen.Preferences.ReferenceSetBehavior
) – Sets a new pmi option on the inherit pmi sub-builderNew in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
ViewStyleInheritPmiBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.