ReferenceSetBehavior Enumeration¶
-
class
NXOpen.Preferences.
ReferenceSetBehavior
¶ Bases:
object
Represents the Reference Set options Enum Members
Enum Member Enum Member Description NotSet No PMI will be inherited if any of the PMI objects has a reference to an object which is not in the active reference set.Partial Inherit only PMI for which all of the referenced objects are in the active reference set.All Inherit all PMI regardless of whether the referenced objects are in the active reference set. Inherited PMI with references to objects outside of the active reference set will be retained.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-