SectionLineBuilderTypes Enumeration

NXOpen.Drawings.SectionLineBuilder.Types is an alias for NXOpen.Drawings.SectionLineBuilderTypes

class NXOpen.Drawings.SectionLineBuilderTypes

Bases: object

Section Line type

Enum Members

Enum Member Enum Member Description
SimpleOrStepped
Half
Revolved
PointToPoint
PointAndAngle
Pictorial
HalfPictorial
Oriented
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.