ShipDraftingViewLinesViewStyle Class¶
-
class
NXOpen.Drawings.
ShipDraftingViewLinesViewStyle
¶ Bases:
object
Represents set of Ship Drafting Lines View Style applicable to drafting views.
Ship Drafting View lines are used for the features in Ship Design To obtain an instance of this class use
Drawings.ViewStyle.ShipDraftingViewLines()
New in version NX10.0.0.
Methods¶
Method | Description |
---|---|
GetColor | Gets line color. |
GetFont | Gets line font. |
GetShipDrawingObject | Get ship drawing object status. |
GetWidth | Gets line width @return |
SetColor | The color of ship line. |
SetFont | The font type of ship line. |
SetShipDrawingObject | Note: The initial values are set based on the file NX_ShipAttribute. |
SetWidth | The width of ship line. |
Enumerations¶
ShipDraftingViewLinesViewStyleLines Enumeration | Line type |
Method Detail¶
GetColor¶
-
ShipDraftingViewLinesViewStyle.
GetColor
¶ Gets line color.
Signature
GetColor(featureName, linesType)
Parameters: - featureName (str) – feature name e.g. decks, bulkheads etc.
- linesType (
NXOpen.Drawings.ShipDraftingViewLinesViewStyleLines
) – visible or hidden line type
Returns: Return type: New in version NX10.0.0.
License requirements: None.
GetFont¶
-
ShipDraftingViewLinesViewStyle.
GetFont
¶ Gets line font.
Signature
GetFont(featureName, linesType)
Parameters: - featureName (str) – feature name e.g. decks, bulkheads etc.
- linesType (
NXOpen.Drawings.ShipDraftingViewLinesViewStyleLines
) – visible or hidden line type
Returns: Return type: New in version NX10.0.0.
License requirements: None.
GetShipDrawingObject¶
-
ShipDraftingViewLinesViewStyle.
GetShipDrawingObject
¶ Get ship drawing object status.
Signature
GetShipDrawingObject(featureName)
Parameters: featureName (str) – feature name e.g. decks, bulkheads etc. Returns: status that determines SLR for the feature Return type: bool New in version NX10.0.0.
License requirements: None.
GetWidth¶
-
ShipDraftingViewLinesViewStyle.
GetWidth
¶ Gets line width
Signature
GetWidth(featureName, linesType)
Parameters: - featureName (str) – feature name e.g. decks, bulkheads etc.
- linesType (
NXOpen.Drawings.ShipDraftingViewLinesViewStyleLines
) – visible or hidden line type
Returns: Return type: New in version NX10.0.0.
License requirements: None.
SetColor¶
-
ShipDraftingViewLinesViewStyle.
SetColor
¶ The color of ship line.
The value should be between UF_OBJ_MIN_COLOR and UF_OBJ_MAX_COLOR.
Signature
SetColor(featureName, linesType, color)
Parameters: - featureName (str) – feature name e.g. decks, bulkheads etc.
- linesType (
NXOpen.Drawings.ShipDraftingViewLinesViewStyleLines
) – visible or hidden line type - color (Id) – Color
New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
SetFont¶
-
ShipDraftingViewLinesViewStyle.
SetFont
¶ The font type of ship line.
Signature
SetFont(featureName, linesType, font)
Parameters: - featureName (str) – feature name e.g. decks, bulkheads etc.
- linesType (
NXOpen.Drawings.ShipDraftingViewLinesViewStyleLines
) – visible or hidden line type - font (
NXOpen.Preferences.Font
) – Font
New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
SetShipDrawingObject¶
-
ShipDraftingViewLinesViewStyle.
SetShipDrawingObject
¶ Note: The initial values are set based on the file NX_ShipAttribute.
xml The status determines the line settings for the ship feature in a view.
Signature
SetShipDrawingObject(featureName, singleLine)
Parameters: - featureName (str) – feature name e.g. decks, bulkheads etc.
- singleLine (bool) – status that determines SLR for the feature
New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
SetWidth¶
-
ShipDraftingViewLinesViewStyle.
SetWidth
¶ The width of ship line.
Signature
SetWidth(featureName, linesType, width)
Parameters: - featureName (str) – feature name e.g. decks, bulkheads etc.
- linesType (
NXOpen.Drawings.ShipDraftingViewLinesViewStyleLines
) – visible or hidden line type - width (
NXOpen.Preferences.Width
) – Width
New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)