ViewStyleVisibleLinesBuilder Class¶
-
class
NXOpen.Drawings.
ViewStyleVisibleLinesBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the VISIBLE LINES tab on the View Style Dialog (Drawings.
ViewStyleVisibleLinesBuilder)
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
VisibleColor | Returns or sets the visible color on the VISIBLE LINES tab of the View Style Dialog |
VisibleFont | Returns or sets the visible font on the VISIBLE LINES tab of the View Style Dialog |
VisibleWidth | Returns or sets the visible width on the VISIBLE LINES tab of the View Style Dialog |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
VisibleColor¶
-
ViewStyleVisibleLinesBuilder.
VisibleColor
¶ Returns or sets the visible color on the VISIBLE LINES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
VisibleColor()
Returns: Returns the visible color that is on the visible lines sub-builder Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisibleColor(visibleColor)
Parameters: visibleColor (Id) – Sets new visible color on the visible lines sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
VisibleFont¶
-
ViewStyleVisibleLinesBuilder.
VisibleFont
¶ Returns or sets the visible font on the VISIBLE LINES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
VisibleFont()
Returns: Returns the visible font that is on the visible lines sub-builder Return type: NXOpen.Preferences.Font
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisibleFont(font)
Parameters: font ( NXOpen.Preferences.Font
) – Sets new visible font on the visible lines sub-builderNew in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
VisibleWidth¶
-
ViewStyleVisibleLinesBuilder.
VisibleWidth
¶ Returns or sets the visible width on the VISIBLE LINES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
VisibleWidth()
Returns: Returns the visible width that is on the visible lines sub-builder Return type: NXOpen.Preferences.Width
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisibleWidth(width)
Parameters: width ( NXOpen.Preferences.Width
) – Sets new visible width on the visible lines sub-builderNew in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
ViewStyleVisibleLinesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.