DrawingSheetBuilderSheetMode Enumeration

NXOpen.Drawings.DrawingSheetBuilder.SheetMode is an alias for NXOpen.Drawings.DrawingSheetBuilderSheetMode

class NXOpen.Drawings.DrawingSheetBuilderSheetMode

Bases: object

the drawing sheet dialog mode

Enum Members

Enum Member Enum Member Description
Create
create mode
Edit
edit mode
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.