ArrowStyleType Enumeration

class NXOpen.Drawings.ArrowStyleType

Bases: object

the arrow style type Enum Members

Enum Member Enum Member Description
Filled
Filled
Closed
Closed
ClosedSolid
Close Solid
Open
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.