PointAndAngleSectionLineBuilder Class

class NXOpen.Drawings.PointAndAngleSectionLineBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.Drawings.PointAndAngleSectionLineBuilder.

This class is used to create or edit a NXOpen.Drawings.PointAndAngleSectionLine. .. versionadded:: NX6.0.0

Deprecated since version NX10.0.0: This API is not supported yet and should not be used.

Properties

Property Description
EndLocation1 Returns or sets the end location 1 which determines the position of the first arrow segment in the section line.
EndLocation2 Returns or sets the end location 2 which determines the position of the second arrow segment in the section line
Leg1 Returns the list of cut segments.
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

EndLocation1

PointAndAngleSectionLineBuilder.EndLocation1

Returns or sets the end location 1 which determines the position of the first arrow segment in the section line.

-------------------------------------

Getter Method

Signature EndLocation1()

Returns:
Return type:NXOpen.Point

New in version NX6.0.0.

Deprecated since version NX10.0.0: This API is not supported yet and should not be used.

License requirements: None.

-------------------------------------

Setter Method

Signature EndLocation1(endLocation1)

Parameters:endLocation1 (NXOpen.Point) –

New in version NX6.0.0.

Deprecated since version NX10.0.0: This API is not supported yet and should not be used.

License requirements: drafting (“DRAFTING”)

EndLocation2

PointAndAngleSectionLineBuilder.EndLocation2

Returns or sets the end location 2 which determines the position of the second arrow segment in the section line

-------------------------------------

Getter Method

Signature EndLocation2()

Returns:
Return type:NXOpen.Point

New in version NX6.0.0.

Deprecated since version NX10.0.0: This API is not supported yet and should not be used.

License requirements: None.

-------------------------------------

Setter Method

Signature EndLocation2(endLocation2)

Parameters:endLocation2 (NXOpen.Point) –

New in version NX6.0.0.

Deprecated since version NX10.0.0: This API is not supported yet and should not be used.

License requirements: drafting (“DRAFTING”)

Leg1

PointAndAngleSectionLineBuilder.Leg1

Returns the list of cut segments.

The list will contain NXOpen.Drawings.SectionLineSegmentBuilder segments of type NXOpen.Drawings.SectionLineSegmentBuilderTypes.Angle only.

Note that the segments are added in the order that they appear in this list.

-------------------------------------

Getter Method

Signature Leg1()

Returns:
Return type:NXOpen.Drawings.SectionLineSegmentBuilderList

New in version NX6.0.0.

Deprecated since version NX10.0.0: This API is not supported yet and should not be used.

License requirements: None.

Method Detail

Validate

PointAndAngleSectionLineBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.