DraftingViewCollectionViewCopyDetailOption Enumeration

NXOpen.Drawings.DraftingViewCollection.ViewCopyDetailOption is an alias for NXOpen.Drawings.DraftingViewCollectionViewCopyDetailOption

class NXOpen.Drawings.DraftingViewCollectionViewCopyDetailOption

Bases: object

Specifies the the view copy mode.

Enum Members

Enum Member Enum Member Description
DetailView
detail view
DuplicateView
duplicate view
ModelView
model view
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.