AutomationTemplateRegionBuilder Class¶
-
class
NXOpen.Drawings.
AutomationTemplateRegionBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Drawings.AutomationTemplateRegionBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
DisplayRegionLabel | Returns or sets the flag to indicate if the display region label should be displayed |
DisplayTemplatePart | Returns or sets the value that determines whether or not regions should be displayed in a non-template part. |
LineColorFontWidth | Returns the value that specifies the color font width of region objectsline |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DisplayRegionLabel¶
-
AutomationTemplateRegionBuilder.
DisplayRegionLabel
¶ Returns or sets the flag to indicate if the display region label should be displayed
-------------------------------------
Getter Method
Signature
DisplayRegionLabel()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayRegionLabel(displayRegionLabel)
Parameters: displayRegionLabel (bool) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
DisplayTemplatePart¶
-
AutomationTemplateRegionBuilder.
DisplayTemplatePart
¶ Returns or sets the value that determines whether or not regions should be displayed in a non-template part.
-------------------------------------
Getter Method
Signature
DisplayTemplatePart()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayTemplatePart(displayTemplatePart)
Parameters: displayTemplatePart (bool) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
LineColorFontWidth¶
-
AutomationTemplateRegionBuilder.
LineColorFontWidth
¶ Returns the value that specifies the color font width of region objectsline
-------------------------------------
Getter Method
Signature
LineColorFontWidth()
Returns: Return type: NXOpen.LineColorFontWidthBuilder
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
AutomationTemplateRegionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.