SectionLineStyleBuilderWidthStyle Enumeration¶
NXOpen.Drawings.SectionLineStyleBuilder.WidthStyle is an alias for NXOpen.Drawings.SectionLineStyleBuilderWidthStyle
-
class
NXOpen.Drawings.
SectionLineStyleBuilderWidthStyle
¶ Bases:
object
This enum represents section line width style type.
Deprecated since version NX10.0.0: This API is not supported yet and should not be used.
Enum Members
Enum Member Enum Member Description Thin ThinNormal NormalThick ThickThicknessOne Width OneThicknessTwo Width TwoThicknessThree Width ThreeThicknessFour Width FourThicknessFive Width FiveThicknessSix Width SixThicknessSeven Width SevenThicknessEight Width EightThicknessNine Width Nine-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-