SheetZoneSettingsBuilder Class

class NXOpen.Drawings.SheetZoneSettingsBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents the Drawing Sheet Zone Setting Style Builder.

New in version NX10.0.0.

Properties

Property Description
ContinueZoneIndexingAcrossSheets Returns or sets the continue zone indexing across sheets
CornerZoneModification Returns or sets the corner zone modification
CreateZoneLabels Returns or sets the create zone labels
CreateZoneMarkings Returns or sets the create zone markings
CreateZones Returns or sets the create zones
HorizontalSize Returns or sets the horizontal size
LabelColor Returns or sets the labels color
LabelFont Returns or sets the labels font
LabelHeight Returns or sets the label height
LabelItalicized Returns or sets the labels font style
LabelWidth Returns or sets the labels width
LabelsToSkip Returns or sets the labels to skip
MarkingHeight Returns or sets the marking height
MarkingLineColorWidth Returns the marking line color width
Origin Returns or sets the origin
Tag Returns the Tag for this object.
VerticalSize Returns or sets the vertical size

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

ContinueZoneIndexingAcrossSheets

SheetZoneSettingsBuilder.ContinueZoneIndexingAcrossSheets

Returns or sets the continue zone indexing across sheets

-------------------------------------

Getter Method

Signature ContinueZoneIndexingAcrossSheets()

Returns:
Return type:bool

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ContinueZoneIndexingAcrossSheets(continueZoneIndexingAcrossSheets)

Parameters:continueZoneIndexingAcrossSheets (bool) –

New in version NX10.0.0.

License requirements: drafting (“DRAFTING”)

CornerZoneModification

SheetZoneSettingsBuilder.CornerZoneModification

Returns or sets the corner zone modification

-------------------------------------

Getter Method

Signature CornerZoneModification()

Returns:
Return type:float

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CornerZoneModification(cornerZoneModification)

Parameters:cornerZoneModification (float) –

New in version NX10.0.0.

License requirements: drafting (“DRAFTING”)

CreateZoneLabels

SheetZoneSettingsBuilder.CreateZoneLabels

Returns or sets the create zone labels

-------------------------------------

Getter Method

Signature CreateZoneLabels()

Returns:
Return type:bool

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CreateZoneLabels(createZoneLabels)

Parameters:createZoneLabels (bool) –

New in version NX10.0.0.

License requirements: drafting (“DRAFTING”)

CreateZoneMarkings

SheetZoneSettingsBuilder.CreateZoneMarkings

Returns or sets the create zone markings

-------------------------------------

Getter Method

Signature CreateZoneMarkings()

Returns:
Return type:bool

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CreateZoneMarkings(createZoneMarkings)

Parameters:createZoneMarkings (bool) –

New in version NX10.0.0.

License requirements: drafting (“DRAFTING”)

CreateZones

SheetZoneSettingsBuilder.CreateZones

Returns or sets the create zones

-------------------------------------

Getter Method

Signature CreateZones()

Returns:
Return type:bool

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CreateZones(createZones)

Parameters:createZones (bool) –

New in version NX10.0.0.

License requirements: drafting (“DRAFTING”)

HorizontalSize

SheetZoneSettingsBuilder.HorizontalSize

Returns or sets the horizontal size

-------------------------------------

Getter Method

Signature HorizontalSize()

Returns:
Return type:float

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature HorizontalSize(horizontalSize)

Parameters:horizontalSize (float) –

New in version NX10.0.0.

License requirements: drafting (“DRAFTING”)

LabelColor

SheetZoneSettingsBuilder.LabelColor

Returns or sets the labels color

-------------------------------------

Getter Method

Signature LabelColor()

Returns:
Return type:int

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature LabelColor(labelColor)

Parameters:labelColor (int) –

New in version NX10.0.0.

License requirements: drafting (“DRAFTING”)

LabelFont

SheetZoneSettingsBuilder.LabelFont

Returns or sets the labels font

-------------------------------------

Getter Method

Signature LabelFont()

Returns:
Return type:int

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature LabelFont(labelFont)

Parameters:labelFont (int) –

New in version NX10.0.0.

License requirements: drafting (“DRAFTING”)

LabelHeight

SheetZoneSettingsBuilder.LabelHeight

Returns or sets the label height

-------------------------------------

Getter Method

Signature LabelHeight()

Returns:
Return type:float

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature LabelHeight(labelHeight)

Parameters:labelHeight (float) –

New in version NX10.0.0.

License requirements: drafting (“DRAFTING”)

LabelItalicized

SheetZoneSettingsBuilder.LabelItalicized

Returns or sets the labels font style

-------------------------------------

Getter Method

Signature LabelItalicized()

Returns:
Return type:bool

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature LabelItalicized(italic)

Parameters:italic (bool) –

New in version NX10.0.0.

License requirements: drafting (“DRAFTING”)

LabelWidth

SheetZoneSettingsBuilder.LabelWidth

Returns or sets the labels width

-------------------------------------

Getter Method

Signature LabelWidth()

Returns:
Return type:int

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature LabelWidth(labelWidth)

Parameters:labelWidth (int) –

New in version NX10.0.0.

License requirements: drafting (“DRAFTING”)

LabelsToSkip

SheetZoneSettingsBuilder.LabelsToSkip

Returns or sets the labels to skip

-------------------------------------

Getter Method

Signature LabelsToSkip()

Returns:
Return type:str

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature LabelsToSkip(labelsToSkip)

Parameters:labelsToSkip (str) –

New in version NX10.0.0.

License requirements: drafting (“DRAFTING”)

MarkingHeight

SheetZoneSettingsBuilder.MarkingHeight

Returns or sets the marking height

-------------------------------------

Getter Method

Signature MarkingHeight()

Returns:
Return type:float

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature MarkingHeight(markingHeight)

Parameters:markingHeight (float) –

New in version NX10.0.0.

License requirements: drafting (“DRAFTING”)

MarkingLineColorWidth

SheetZoneSettingsBuilder.MarkingLineColorWidth

Returns the marking line color width

-------------------------------------

Getter Method

Signature MarkingLineColorWidth()

Returns:
Return type:NXOpen.LineColorFontWidthBuilder

New in version NX10.0.0.

License requirements: None.

Origin

SheetZoneSettingsBuilder.Origin

Returns or sets the origin

-------------------------------------

Getter Method

Signature Origin()

Returns:
Return type:NXOpen.Drawings.ZoneOrigin

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Origin(origin)

Parameters:origin (NXOpen.Drawings.ZoneOrigin) –

New in version NX10.0.0.

License requirements: drafting (“DRAFTING”)

VerticalSize

SheetZoneSettingsBuilder.VerticalSize

Returns or sets the vertical size

-------------------------------------

Getter Method

Signature VerticalSize()

Returns:
Return type:float

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature VerticalSize(verticalSize)

Parameters:verticalSize (float) –

New in version NX10.0.0.

License requirements: drafting (“DRAFTING”)

Method Detail

Validate

SheetZoneSettingsBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.