BrokenViewBuilderBreakLineStyle Enumeration¶
NXOpen.Drawings.BrokenViewBuilder.BreakLineStyle is an alias for NXOpen.Drawings.BrokenViewBuilderBreakLineStyle
-
class
NXOpen.Drawings.
BrokenViewBuilderBreakLineStyle
¶ Bases:
object
Break Line Type
Enum Members
Enum Member Enum Member Description Simple SimpleStraight StraightSawtooth SawtoothLongBreak LongBreakTubular TubularSolidTubular Solid TubularSolidRod Solid RodJigsaw JigsawWood WoodCopyCurve Copy of the existing curveTemplateCurve Template, based on the existing curve-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-