SelectModelViewBuilder Class

class NXOpen.Drawings.SelectModelViewBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a Select Model View builder that selects a model view

New in version NX6.0.0.

Properties

Property Description
SelectedView Returns or sets the selected view
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

SelectedView

SelectModelViewBuilder.SelectedView

Returns or sets the selected view

-------------------------------------

Getter Method

Signature SelectedView()

Returns:
Return type:NXOpen.ModelingView

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SelectedView(view)

Parameters:view (NXOpen.ModelingView) –

New in version NX6.0.0.

License requirements: drafting (“DRAFTING”)

Method Detail

Validate

SelectModelViewBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.