AddRemoveBoxViewBuilderModeType Enumeration

NXOpen.Drawings.AddRemoveBoxViewBuilder.ModeType is an alias for NXOpen.Drawings.AddRemoveBoxViewBuilderModeType

class NXOpen.Drawings.AddRemoveBoxViewBuilderModeType

Bases: object

Mode type

Enum Members

Enum Member Enum Member Description
Add
Add mode
Remove
Remove mode
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.