AutoPointBuilderInterferenceDetails Enumeration |
Settings to indicate whether an interference is near an existing weld point. |
AutoPointBuilderTypes Enumeration |
Settings to indicate whether new features should be created, or if features will be reused. |
CharacteristicsBuilderType Enumeration |
The custom type of the datum specified for creation. |
CharacteristicsValueBuilderType Enumeration |
Settings to indicate the type of value contained in the attribute. |
ConnectionFinderBuilderFilterTypes Enumeration |
Filter values to control Save All processing. |
DatumCommonBuilderControlMethodTypes Enumeration |
Settings for the method used to define the control direction. |
DatumCommonBuilderCreationDirectionMethods Enumeration |
Settings to define the creation direction. |
DatumCommonBuilderCustomTypes Enumeration |
The custom type of the datum specified for creation. |
DatumCommonBuilderSolidTypes Enumeration |
Settings for defining the solid type to create for the datum object. |
DatumSurfaceBuilderTypes Enumeration |
Settings to indicate the construction type used for the datum surface. |
EasyPatternBuilderHemMethodTypes Enumeration |
Indicates the method to use to compute the hem vector location. |
EasyPatternBuilderPlaneMethodTypes Enumeration |
The plane to cut sections in to determine placement measurement patterns. |
EasyPatternBuilderSpacingMethodTypes Enumeration |
Indicates whether planes should be cut a grid lines, or if a single plane should be used. |
EasyPatternBuilderTypes Enumeration |
Controls the type of pattern. |
EdgePrepValuesBuilderApply Enumeration |
Option to indicate how the values are to be updated. |
EdgePrepValuesBuilderOption Enumeration |
Option to indicate how the values are to be used. |
ExportWeldBuilderAttributeOriginType Enumeration |
the Attribute Origin enum |
ExportWeldBuilderOutputType Enumeration |
the Output Type enum |
FilletBuilderEnumConstructionMethod Enumeration |
the options for which construction method to use. |
FilletBuilderEnumContour Enumeration |
the Contour enum. |
FilletBuilderEnumExtendEdges Enumeration |
the options for populating the edge selections. |
FilletBuilderEnumExtensionMethod Enumeration |
the Extension enum. |
FilletBuilderEnumSkipWeldMethod Enumeration |
the Skipweld enum. |
FilletBuilderEnumWeldingType Enumeration |
the WeldingType enum. |
InformationBuilderAttributeOriginType Enumeration |
the Object Type enum |
JointExitBuilderBodySide Enumeration |
Settings to indicate the side the positions should be applied to. |
JointExitBuilderPositions Enumeration |
Settings to indicate the desired position of edge preporation thickness and angle. |
JointmarkBuilderConnectedPanelTypes Enumeration |
The type of sheets to create |
JointmarkBuilderMethod Enumeration |
The type of construction method for creating Jointmark |
JointmarkBuilderOrientationMethodTypes Enumeration |
The type of orientation method for defining the default coordinate system. |
JointmarkBuilderProjectionDirectionOptions Enumeration |
The projection direction used to project points onto the reference sheet |
JointmarkBuilderReferenceSheetTypes Enumeration |
The type of sheets to create |
JointmarkGuideBuilderLocation Enumeration |
The type of guide curve |
JointmarkGuideBuilderSpaceMethod Enumeration |
Options for Spacing Method |
JointmarkGuideBuilderSpaceOption Enumeration |
Spacing Option |
JointmarkPointsBuilderPointPosition Enumeration |
The point classification |
OutputType Enumeration |
Settings for output type |
PlugSlotBuilderArcProcessEnum Enumeration |
arc process for the weld feature |
PlugSlotBuilderEnumContour Enumeration |
contour type |
PointMarkBuilderWeldTypes Enumeration |
The weld type to create. |
SurfaceWeldBuilderDestinationTypes Enumeration |
The option specifying where the surface weld feature should be created. |
UserDefinedWeldBuilderWeldTypes Enumeration |
Weld types for 4GD classes. |
WeldAdvisorCheckerType Enumeration |
the type of checker |
WeldAdvisorCustomerDefault Enumeration |
the customer default value types |
WeldArcMethod Enumeration |
Settings for output type |
WeldAttribType Enumeration |
the type of attribute |
WeldBeadBuilderBeadLocationMethod Enumeration |
Settings to indicate the desired location of the bead. |
WeldBeadBuilderOutputTypes Enumeration |
Settings to indicate the update behaviour of the bead feature |
WeldBeadBuilderTypes Enumeration |
Settings to indicate the sweep shape of the bead. |
WeldBeadPathBuilderOffsetMethodType Enumeration |
Settings to indicate the desired offset method. |
WeldBeadSizeBuilderSize Enumeration |
Settings to indicate which standard size to use from the customer defaults file. |
WeldBeadSizeBuilderTriangleMethodType Enumeration |
Settings to indicate the type of method used to build a triangle shape. |
WeldBeadSizeBuilderTriangleTypes Enumeration |
Settings to indicate the type of triangle. |
WeldContourShape Enumeration |
Top contour shape |
WeldCreationDirection Enumeration |
the type of creation direction |
WeldCustom Enumeration |
Settings for output solid type |
WeldDatumControlDirection Enumeration |
the control direction for datum |
WeldFacesetIndex Enumeration |
the index of user picked face sets |
WeldFeatureOutput Enumeration |
Feature output |
WeldFeatureSetType Enumeration |
the feature set types |
WeldFillBuilderBoundaryMethodType Enumeration |
Defines whether the initial boundary of the fill pattern is defined by a two point rectangle or a curve. |
WeldFillBuilderWidthAlongType Enumeration |
Defines the direction the fill strip’s length is aligned |
WeldGrooveBuilderContour Enumeration |
The options for Contour Type |
WeldGrooveBuilderEdge Enumeration |
A value indicating whether the edges have been prepared |
WeldGrooveBuilderPrepare Enumeration |
The type of edges to be prepared |
WeldGrooveBuilderSkipWeldMethod Enumeration |
The options for creating Skip Weld |
WeldGrooveBuilderTaper Enumeration |
The type of Taper Method |
WeldGrooveBuilderTypes Enumeration |
The types of Groove to create |
WeldGrooveExtension Enumeration |
Groove Extension Type |
WeldGrooveShape Enumeration |
Groove Weld Section type |
WeldGrooveType Enumeration |
Groove Creation Type |
WeldGroupIdColor Enumeration |
the group id color indexes |
WeldJointBuilderApplication Enumeration |
Application where joints are created. |
WeldJointBuilderCoordinateSystem Enumeration |
Coordinate system specification. |
WeldJointBuilderDestinationTypes Enumeration |
Where to create new joints. |
WeldJointBuilderSplitTypes Enumeration |
Joint splitting options. |
WeldJointBuilderTypes Enumeration |
Creation method. |
WeldJointBuilderWeldTypes Enumeration |
Weld types. |
WeldLabelBuilderOrientationPlaneType Enumeration |
This represents the Orientation Plane Type. |
WeldMeasurementSizeMethod Enumeration |
the size method for measurement |
WeldObjectBuilderCommandName Enumeration |
Commands that a callback will be invoked after dialog completion. |
WeldOverlapStatus Enumeration |
the create status for overlap |
WeldParasetLocation Enumeration |
the index of user picked refsheet location |
WeldPmiBuilderOrientationPlaneType Enumeration |
This represents the Orientation Plane Type. |
WeldPointDirection Enumeration |
Spot direction |
WeldPointExitBuilderCommandName Enumeration |
The command name used for the newly created features. |
WeldPointExitBuilderMethodUsed Enumeration |
The method use to create the features. |
WeldPointExtendMethod Enumeration |
Offset curve extend method |
WeldPointLocation Enumeration |
Settings locating spot welds using guide curves/edges |
WeldPointMethod Enumeration |
Settings for method |
WeldPointReferenceSheetType Enumeration |
Settings for the reference sheet |
WeldPointSpacingMethod Enumeration |
Guide spacing method |
WeldPrepareEdges Enumeration |
Settings for prepare edges |
WeldProjectionMethod Enumeration |
Settings project method type |
WeldRootUpdate Enumeration |
Arc process type |
WeldSelectionType Enumeration |
the type of selction |
WeldSpacingCalcMethod Enumeration |
Settings spacing method type |
WeldTaperMethod Enumeration |
Settings for groove taper method |