WeldAdvisorCustomerDefault Enumeration

class NXOpen.Weld.WeldAdvisorCustomerDefault

Bases: object

the customer default value types Enum Members

Enum Member Enum Member Description
ResistanceSpot
Resistance Spot
ArcSpot
Arc Spot
Clinch
Clinch
Dollop
Dollop
WeldNut
Weld Nut
WeldStud
Weld Stud
Custom1Point
Custom1 Point
Custom2Point
Custom2 Point
Custom3Point
Custom3 Point
Custom4Point
Custom4 Point
Custom5Point
Custom5 Point
Datum
datum, used for implementing weld advisor parameters
Measurement
measurement, used for implementing weld advisor parameters
Num
number of types
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.