LocatorReferenceBuilder Class¶
-
class
NXOpen.Weld.
LocatorReferenceBuilder
¶ Bases:
NXOpen.Builder
This class is used by “Locator Reference” to add the additional component for a weld datum DF.
When commit is called, the selected additional components will be added to weld datum parms.
To create a new instance of this class, use
NXOpen.Weld.WeldManager.CreateLocatorReferenceBuilder()
New in version NX10.0.2.
Properties¶
Property | Description |
---|---|
AdditionalReferences | Returns the additional references |
SelectLocator | Returns the selecte locator |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetAdditionalReferenceFromFeature | Set additional references. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AdditionalReferences¶
-
LocatorReferenceBuilder.
AdditionalReferences
¶ Returns the additional references
-------------------------------------
Getter Method
Signature
AdditionalReferences()
Returns: Return type: NXOpen.Assemblies.SelectComponentList
New in version NX10.0.2.
License requirements: None.
SelectLocator¶
-
LocatorReferenceBuilder.
SelectLocator
¶ Returns the selecte locator
-------------------------------------
Getter Method
Signature
SelectLocator()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX10.0.2.
License requirements: None.
Method Detail¶
SetAdditionalReferenceFromFeature¶
-
LocatorReferenceBuilder.
SetAdditionalReferenceFromFeature
¶ Set additional references.
Use to set additional references from feature.
Signature
SetAdditionalReferenceFromFeature(additionalReference)
Parameters: additionalReference ( NXOpen.Features.Feature
) –New in version NX10.0.2.
License requirements: ugweld (“UG WELD”)
Validate¶
-
LocatorReferenceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.