EdgePrepValuesBuilderApply Enumeration¶
NXOpen.Weld.EdgePrepValuesBuilder.Apply is an alias for NXOpen.Weld.EdgePrepValuesBuilderApply
-
class
NXOpen.Weld.
EdgePrepValuesBuilderApply
¶ Bases:
object
Option to indicate how the values are to be updated.
Enum Members
Enum Member Enum Member Description ToAllValues Update all values of each selected joint.ToChangedValuesOnly Update only the changed values to each selected joint.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-