EasyPatternBuilderTypes Enumeration

NXOpen.Weld.EasyPatternBuilder.Types is an alias for NXOpen.Weld.EasyPatternBuilderTypes

class NXOpen.Weld.EasyPatternBuilderTypes

Bases: object

Controls the type of pattern.

Enum Members

Enum Member Enum Member Description
TrimAndSurface
Trim vector and surface vectors.
HemAndSurface
Hem vector and surface vectors.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.