WeldPointMethod Enumeration

class NXOpen.Weld.WeldPointMethod

Bases: object

Settings for method Enum Members

Enum Member Enum Member Description
Multiple
use guide curve(s) or edge(s) to generate spot weld points
Single
use point constructor to generate spot weld points
Mirror
mirror existing points
Translate
translate existing points
FromPoints
create fix/single/none points using existing points
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.