JointExitBuilderPositions Enumeration¶
NXOpen.Weld.JointExitBuilder.Positions is an alias for NXOpen.Weld.JointExitBuilderPositions
-
class
NXOpen.Weld.
JointExitBuilderPositions
¶ Bases:
object
Settings to indicate the desired position of edge preporation thickness and angle.
Enum Members
Enum Member Enum Member Description UpperChamfer the upper chamfer positionUpper the upper positionMiddle the middle positionLower the lower positionLowerChamfer the lower chamfer position-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-