FilletBuilder Class¶
-
class
NXOpen.Weld.
FilletBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Weld.Fillet
builder.To create a new instance of this class, use
NXOpen.Weld.WeldManager.CreateFilletBuilder()
Default values.
Property Value AddCosmeticEnd 0 AllowBroken 0 AssignWeldPMI 0 Associative 1 ContourHeight.Value 1.875 (millimeters part), .073818 (inches part) ContourType None EnumMethod NumberLength ExtendEdges Manual ExtensionDistance.Value 0.0254 (millimeters part), 0.001 (inches part) ExtensionMethod Automatic FaceFillGapDistance 0.0 (millimeters part), 0.0 (inches part) FieldWeld 0 FilletType T FirstLeg.Value 6.25 (millimeters part), .246062 (inches part) NumberOfWelds.Value 3 SecondLeg.Value 6.25 (millimeters part), .246062 (inches part) SegmentLength.Value 3 (millimeters part), .118110 (inches part) Spacing.Value 3 (millimeters part), .118110 (inches part) ThroatThickToggle 0 ToggleCreateSkipWelds 0 ToggleRecreateDeletedWelds 0 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AddCosmeticEnd | Returns or sets the value identify if a cosmtic end should be added to each end of the fillet. |
AllowBroken | Returns or sets the toggle to allow broken link. |
AssignWeldPMI | Returns or sets the toggle to assign weld pmi. |
Associative | Returns or sets the value identify if WAVE links should remain unbroken. |
ConstructionMethod | Returns or sets the value for determining the construction method. |
ContourHeight | Returns the linear dimension contour height. |
ContourType | Returns or sets the contour. |
DirectToggle | Returns or sets the toggle to change direction. |
DirectionVector1 | Returns or sets the face normal direction. |
DirectionVector2 | Returns or sets the face normal direction for the second face. |
DistTolerance | Returns or sets the distance tolerance. |
EdgeSet1 | Returns the edge set1. |
EdgeSet2 | Returns the edge set2. |
EndDist | Returns the on path dimension end distance. |
EndVector | Returns or sets the end direction reversed or not. |
EnumMethod | Returns or sets the enum method for skip welds. |
ExtendEdges | Returns or sets the value for how to populate the edge sets. |
ExtensionDistance | Returns the linear dimension extension distance. |
ExtensionMethod | Returns or sets the extension method. |
FaceFillGapDistance | Returns or sets the distance the fillet will span when there are gaps in the sheet definition. |
FaceSet1 | Returns the face set1. |
FaceSet2 | Returns the face set2. |
FieldWeld | Returns or sets the field weld. |
FilletType | Returns or sets the fillet type. |
FirstLeg | Returns the linear dimension first leg. |
NumberOfWelds | Returns the expression number indicates number of welds in skip welds. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Pmi | Returns or sets the pmi symbol. |
SecondLeg | Returns the linear dimension second leg. |
SeedFace1 | Returns or sets the first seed face. |
SeedFace2 | Returns or sets the second seed face. |
SeedPoint1 | Returns or sets the point on the first face. |
SeedPoint2 | Returns or sets the point on the second face. |
SegmentLength | Returns the linear dimension length indicates segment length for each weld. |
Spacing | Returns the linear dimension spacing indicates distance between each weld. |
StartDist | Returns the on path dimension start distance. |
StartVector | Returns or sets the start direction reversed or not. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
ThroatThickToggle | Returns or sets the toggle throat thickness. |
ToggleCreateSkipWelds | Returns or sets the toggle to create skip welds. |
ToggleRecreateDeletedWelds | Returns or sets the toggle to recreate deleted welds. |
Uparameter1 | Returns or sets the u parameter for first face. |
Uparameter2 | Returns or sets the u parameter for second face. |
Vparameter1 | Returns or sets the v parameter for first face. |
Vparameter2 | Returns or sets the v parameter for second face. |
WeldingCharacteristics | Returns the welding characteristics. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FilletBuilderEnumConstructionMethod Enumeration | the options for which construction method to use. |
FilletBuilderEnumContour Enumeration | the Contour enum. |
FilletBuilderEnumExtendEdges Enumeration | the options for populating the edge selections. |
FilletBuilderEnumExtensionMethod Enumeration | the Extension enum. |
FilletBuilderEnumSkipWeldMethod Enumeration | the Skipweld enum. |
FilletBuilderEnumWeldingType Enumeration | the WeldingType enum. |
Property Detail¶
AddCosmeticEnd¶
-
FilletBuilder.
AddCosmeticEnd
¶ Returns or sets the value identify if a cosmtic end should be added to each end of the fillet.
-------------------------------------
Getter Method
Signature
AddCosmeticEnd()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AddCosmeticEnd(addCosmeticEnd)
Parameters: addCosmeticEnd (bool) – New in version NX10.0.0.
License requirements: ugweld (“UG WELD”)
AllowBroken¶
-
FilletBuilder.
AllowBroken
¶ Returns or sets the toggle to allow broken link.
-------------------------------------
Getter Method
Signature
AllowBroken()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AllowBroken(allowBroken)
Parameters: allowBroken (bool) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
AssignWeldPMI¶
-
FilletBuilder.
AssignWeldPMI
¶ Returns or sets the toggle to assign weld pmi.
-------------------------------------
Getter Method
Signature
AssignWeldPMI()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AssignWeldPMI(assignWeldPMI)
Parameters: assignWeldPMI (bool) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
Associative¶
-
FilletBuilder.
Associative
¶ Returns or sets the value identify if WAVE links should remain unbroken.
-------------------------------------
Getter Method
Signature
Associative()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Associative(associative)
Parameters: associative (bool) – New in version NX10.0.0.
License requirements: ugweld (“UG WELD”)
ConstructionMethod¶
-
FilletBuilder.
ConstructionMethod
¶ Returns or sets the value for determining the construction method.
Default method should be used for all conditions, unless you know the situation if for the roll around condition.
-------------------------------------
Getter Method
Signature
ConstructionMethod()
Returns: Return type: NXOpen.Weld.FilletBuilderEnumConstructionMethod
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConstructionMethod(constructionMethod)
Parameters: constructionMethod ( NXOpen.Weld.FilletBuilderEnumConstructionMethod
) –New in version NX10.0.0.
License requirements: ugweld (“UG WELD”)
ContourHeight¶
-
FilletBuilder.
ContourHeight
¶ Returns the linear dimension contour height.
-------------------------------------
Getter Method
Signature
ContourHeight()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
ContourType¶
-
FilletBuilder.
ContourType
¶ Returns or sets the contour.
-------------------------------------
Getter Method
Signature
ContourType()
Returns: Return type: NXOpen.Weld.FilletBuilderEnumContour
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ContourType(contour)
Parameters: contour ( NXOpen.Weld.FilletBuilderEnumContour
) –New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
DirectToggle¶
-
FilletBuilder.
DirectToggle
¶ Returns or sets the toggle to change direction.
-------------------------------------
Getter Method
Signature
DirectToggle()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DirectToggle(directToggle)
Parameters: directToggle (bool) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
DirectionVector1¶
-
FilletBuilder.
DirectionVector1
¶ Returns or sets the face normal direction.
-------------------------------------
Getter Method
Signature
DirectionVector1()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DirectionVector1(directionVector1)
Parameters: directionVector1 (bool) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
DirectionVector2¶
-
FilletBuilder.
DirectionVector2
¶ Returns or sets the face normal direction for the second face.
-------------------------------------
Getter Method
Signature
DirectionVector2()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DirectionVector2(directionVector2)
Parameters: directionVector2 (bool) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
DistTolerance¶
-
FilletBuilder.
DistTolerance
¶ Returns or sets the distance tolerance.
-------------------------------------
Getter Method
Signature
DistTolerance()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistTolerance(distTolerance)
Parameters: distTolerance (float) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
EdgeSet1¶
-
FilletBuilder.
EdgeSet1
¶ Returns the edge set1.
-------------------------------------
Getter Method
Signature
EdgeSet1()
Returns: Return type: NXOpen.Section
New in version NX8.0.0.
License requirements: None.
EdgeSet2¶
-
FilletBuilder.
EdgeSet2
¶ Returns the edge set2.
-------------------------------------
Getter Method
Signature
EdgeSet2()
Returns: Return type: NXOpen.Section
New in version NX8.0.0.
License requirements: None.
EndDist¶
-
FilletBuilder.
EndDist
¶ Returns the on path dimension end distance.
-------------------------------------
Getter Method
Signature
EndDist()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX8.0.0.
License requirements: None.
EndVector¶
-
FilletBuilder.
EndVector
¶ Returns or sets the end direction reversed or not.
-------------------------------------
Getter Method
Signature
EndVector()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndVector(endVector)
Parameters: endVector (bool) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
EnumMethod¶
-
FilletBuilder.
EnumMethod
¶ Returns or sets the enum method for skip welds.
-------------------------------------
Getter Method
Signature
EnumMethod()
Returns: Return type: NXOpen.Weld.FilletBuilderEnumSkipWeldMethod
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumMethod(enumMethod)
Parameters: enumMethod ( NXOpen.Weld.FilletBuilderEnumSkipWeldMethod
) –New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
ExtendEdges¶
-
FilletBuilder.
ExtendEdges
¶ Returns or sets the value for how to populate the edge sets.
-------------------------------------
Getter Method
Signature
ExtendEdges()
Returns: Return type: NXOpen.Weld.FilletBuilderEnumExtendEdges
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtendEdges(extendEdges)
Parameters: extendEdges ( NXOpen.Weld.FilletBuilderEnumExtendEdges
) –New in version NX10.0.0.
License requirements: ugweld (“UG WELD”)
ExtensionDistance¶
-
FilletBuilder.
ExtensionDistance
¶ Returns the linear dimension extension distance.
-------------------------------------
Getter Method
Signature
ExtensionDistance()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
ExtensionMethod¶
-
FilletBuilder.
ExtensionMethod
¶ Returns or sets the extension method.
-------------------------------------
Getter Method
Signature
ExtensionMethod()
Returns: Return type: NXOpen.Weld.FilletBuilderEnumExtensionMethod
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtensionMethod(extensionMethod)
Parameters: extensionMethod ( NXOpen.Weld.FilletBuilderEnumExtensionMethod
) –New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
FaceFillGapDistance¶
-
FilletBuilder.
FaceFillGapDistance
¶ Returns or sets the distance the fillet will span when there are gaps in the sheet definition.
-------------------------------------
Getter Method
Signature
FaceFillGapDistance()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FaceFillGapDistance(faceFillGapDistance)
Parameters: faceFillGapDistance (float) – New in version NX10.0.0.
License requirements: ugweld (“UG WELD”)
FaceSet1¶
-
FilletBuilder.
FaceSet1
¶ Returns the face set1.
-------------------------------------
Getter Method
Signature
FaceSet1()
Returns: Return type: NXOpen.ScCollector
New in version NX8.0.0.
License requirements: None.
FaceSet2¶
-
FilletBuilder.
FaceSet2
¶ Returns the face set2.
-------------------------------------
Getter Method
Signature
FaceSet2()
Returns: Return type: NXOpen.ScCollector
New in version NX8.0.0.
License requirements: None.
FieldWeld¶
-
FilletBuilder.
FieldWeld
¶ Returns or sets the field weld.
-------------------------------------
Getter Method
Signature
FieldWeld()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FieldWeld(fieldWeld)
Parameters: fieldWeld (bool) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
FilletType¶
-
FilletBuilder.
FilletType
¶ Returns or sets the fillet type.
-------------------------------------
Getter Method
Signature
FilletType()
Returns: Return type: NXOpen.Weld.FilletBuilderEnumWeldingType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FilletType(filletType)
Parameters: filletType ( NXOpen.Weld.FilletBuilderEnumWeldingType
) –New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
FirstLeg¶
-
FilletBuilder.
FirstLeg
¶ Returns the linear dimension first leg.
-------------------------------------
Getter Method
Signature
FirstLeg()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
NumberOfWelds¶
-
FilletBuilder.
NumberOfWelds
¶ Returns the expression number indicates number of welds in skip welds.
-------------------------------------
Getter Method
Signature
NumberOfWelds()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Pmi¶
-
FilletBuilder.
Pmi
¶ Returns or sets the pmi symbol.
-------------------------------------
Getter Method
Signature
Pmi()
Returns: Return type: NXOpen.NXObject
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Pmi(pmi)
Parameters: pmi ( NXOpen.NXObject
) –New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
SecondLeg¶
-
FilletBuilder.
SecondLeg
¶ Returns the linear dimension second leg.
-------------------------------------
Getter Method
Signature
SecondLeg()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
SeedFace1¶
-
FilletBuilder.
SeedFace1
¶ Returns or sets the first seed face.
-------------------------------------
Getter Method
Signature
SeedFace1()
Returns: Return type: NXOpen.Face
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SeedFace1(seedFace1)
Parameters: seedFace1 ( NXOpen.Face
) –New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
SeedFace2¶
-
FilletBuilder.
SeedFace2
¶ Returns or sets the second seed face.
-------------------------------------
Getter Method
Signature
SeedFace2()
Returns: Return type: NXOpen.Face
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SeedFace2(seedFace2)
Parameters: seedFace2 ( NXOpen.Face
) –New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
SeedPoint1¶
-
FilletBuilder.
SeedPoint1
¶ Returns or sets the point on the first face.
-------------------------------------
Getter Method
Signature
SeedPoint1()
Returns: Return type: NXOpen.Point3d
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SeedPoint1(seedPoint1)
Parameters: seedPoint1 ( NXOpen.Point3d
) –New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
SeedPoint2¶
-
FilletBuilder.
SeedPoint2
¶ Returns or sets the point on the second face.
-------------------------------------
Getter Method
Signature
SeedPoint2()
Returns: Return type: NXOpen.Point3d
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SeedPoint2(seedPoint1)
Parameters: seedPoint1 ( NXOpen.Point3d
) –New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
SegmentLength¶
-
FilletBuilder.
SegmentLength
¶ Returns the linear dimension length indicates segment length for each weld.
-------------------------------------
Getter Method
Signature
SegmentLength()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Spacing¶
-
FilletBuilder.
Spacing
¶ Returns the linear dimension spacing indicates distance between each weld.
-------------------------------------
Getter Method
Signature
Spacing()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
StartDist¶
-
FilletBuilder.
StartDist
¶ Returns the on path dimension start distance.
-------------------------------------
Getter Method
Signature
StartDist()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX8.0.0.
License requirements: None.
StartVector¶
-
FilletBuilder.
StartVector
¶ Returns or sets the start direction reversed or not.
-------------------------------------
Getter Method
Signature
StartVector()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartVector(startVector)
Parameters: startVector (bool) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
ThroatThickToggle¶
-
FilletBuilder.
ThroatThickToggle
¶ Returns or sets the toggle throat thickness.
-------------------------------------
Getter Method
Signature
ThroatThickToggle()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThroatThickToggle(throatThickToggle)
Parameters: throatThickToggle (bool) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
ToggleCreateSkipWelds¶
-
FilletBuilder.
ToggleCreateSkipWelds
¶ Returns or sets the toggle to create skip welds.
-------------------------------------
Getter Method
Signature
ToggleCreateSkipWelds()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToggleCreateSkipWelds(toggleCreateSkipWelds)
Parameters: toggleCreateSkipWelds (bool) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
ToggleRecreateDeletedWelds¶
-
FilletBuilder.
ToggleRecreateDeletedWelds
¶ Returns or sets the toggle to recreate deleted welds.
-------------------------------------
Getter Method
Signature
ToggleRecreateDeletedWelds()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToggleRecreateDeletedWelds(toggleRecreateDeletedWelds)
Parameters: toggleRecreateDeletedWelds (bool) – New in version NX8.0.0.
License requirements: ugweld (“UG WELD”)
Uparameter1¶
-
FilletBuilder.
Uparameter1
¶ Returns or sets the u parameter for first face.
-------------------------------------
Getter Method
Signature
Uparameter1()
Returns: Return type: float New in version NX8.0.0.
Deprecated since version NX10.0.0: Removed with no replacement.
License requirements: None.
-------------------------------------
Setter Method
Signature
Uparameter1(u1)
Parameters: u1 (float) – New in version NX8.0.0.
Deprecated since version NX10.0.0: Removed with no replacement.
License requirements: ugweld (“UG WELD”)
Uparameter2¶
-
FilletBuilder.
Uparameter2
¶ Returns or sets the u parameter for second face.
-------------------------------------
Getter Method
Signature
Uparameter2()
Returns: Return type: float New in version NX8.0.0.
Deprecated since version NX10.0.0: Removed with no replacement.
License requirements: None.
-------------------------------------
Setter Method
Signature
Uparameter2(u2)
Parameters: u2 (float) – New in version NX8.0.0.
Deprecated since version NX10.0.0: Removed with no replacement.
License requirements: ugweld (“UG WELD”)
Vparameter1¶
-
FilletBuilder.
Vparameter1
¶ Returns or sets the v parameter for first face.
-------------------------------------
Getter Method
Signature
Vparameter1()
Returns: Return type: float New in version NX8.0.0.
Deprecated since version NX10.0.0: Removed with no replacement.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vparameter1(v1)
Parameters: v1 (float) – New in version NX8.0.0.
Deprecated since version NX10.0.0: Removed with no replacement.
License requirements: ugweld (“UG WELD”)
Vparameter2¶
-
FilletBuilder.
Vparameter2
¶ Returns or sets the v parameter for second face.
-------------------------------------
Getter Method
Signature
Vparameter2()
Returns: Return type: float New in version NX8.0.0.
Deprecated since version NX10.0.0: Removed with no replacement.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vparameter2(v2)
Parameters: v2 (float) – New in version NX8.0.0.
Deprecated since version NX10.0.0: Removed with no replacement.
License requirements: ugweld (“UG WELD”)
WeldingCharacteristics¶
-
FilletBuilder.
WeldingCharacteristics
¶ Returns the welding characteristics.
-------------------------------------
Getter Method
Signature
WeldingCharacteristics()
Returns: Return type: NXOpen.Weld.CharacteristicsBuilder
New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
FilletBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.