CharacteristicsBuilder Class¶
-
class
NXOpen.Weld.
CharacteristicsBuilder
¶ Bases:
NXOpen.Builder
This builder allows you to define the attribute values to be set on the output of the weld feature.
To create a new instance of this class, use
NXOpen.Weld.WeldManager.CreateCharacteristicsBuilder()
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
InheritObject | Returns the selection object containing data that is used to define the attribute values. |
Selected | Returns or sets the selected characteristic value. |
SelectionList | Returns the list of potential attributes and objects selected for this weld feature. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
ApplyAttributes | Apply the selected attributes to the objects. |
ApplyAttributesToSelected | Apply the selected attributes to the objects that were selected. |
AreAttributesDefault | Returns true if the characteristics builder contains all attributes with default values. |
ChangeFeatureType | Change the type of feature defining the attributes. |
Commit | Commits any edits that have been applied to the builder. |
CopyAttributesFromObject | Copy the attributes that are on the object to the selection. |
CopyAttributesFromObjectForPaint | Copies the attributes that are on the object to the selection for paint. |
CopyNonActiveAttributesFromObject | Copy the non active attributes that are on the object to the selection. |
CreateSelectionSet | Create a new selection set and add it to the list. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
DoesObjectHaveAttributes | Copy the attributes that are on the object to the selection and returns a flag indicating whether the object actually has attributes. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
HasActiveValues | Returns true if the characteristics builder has any active values. |
InheritAttributesFromObject | Inherit the attributes that are on the object to the selection. |
RemoveAllAttributes | Remove all attributes from the objects. |
RemoveInheritedAttributes | Remove any attributes that are inherited from other objects (for example, edges). |
SetAllAttributesChanged | Sets all attributes to be changed. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CharacteristicsBuilderType Enumeration | The custom type of the datum specified for creation. |
Property Detail¶
InheritObject¶
-
CharacteristicsBuilder.
InheritObject
¶ Returns the selection object containing data that is used to define the attribute values.
-------------------------------------
Getter Method
Signature
InheritObject()
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.5.0.
License requirements: None.
Selected¶
-
CharacteristicsBuilder.
Selected
¶ Returns or sets the selected characteristic value.
-------------------------------------
Getter Method
Signature
Selected()
Returns: Return type: NXOpen.Weld.CharacteristicsValueBuilder
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Selected(valueBuilder)
Parameters: valueBuilder ( NXOpen.Weld.CharacteristicsValueBuilder
) –New in version NX7.5.0.
License requirements: None.
SelectionList¶
-
CharacteristicsBuilder.
SelectionList
¶ Returns the list of potential attributes and objects selected for this weld feature.
-------------------------------------
Getter Method
Signature
SelectionList()
Returns: Return type: NXOpen.NXObjectList
New in version NX7.5.0.
License requirements: None.
Method Detail¶
ApplyAttributes¶
-
CharacteristicsBuilder.
ApplyAttributes
¶ Apply the selected attributes to the objects.
Signature
ApplyAttributes(objects)
Parameters: objects (list of NXOpen.NXObject
) – The objects to apply the attributes to.New in version NX7.5.0.
License requirements: None.
ApplyAttributesToSelected¶
-
CharacteristicsBuilder.
ApplyAttributesToSelected
¶ Apply the selected attributes to the objects that were selected.
Signature
ApplyAttributesToSelected()
New in version NX7.5.0.
License requirements: None.
AreAttributesDefault¶
-
CharacteristicsBuilder.
AreAttributesDefault
¶ Overloaded method AreAttributesDefault
AreAttributesDefault(weldType)
AreAttributesDefault(charxType)
-------------------------------------
Returns true if the characteristics builder contains all attributes with default values.
Signature
AreAttributesDefault(weldType)
Parameters: weldType (int) – The type of welding feature being processed, see uf_weld_types.h. Returns: Return type: bool New in version NX8.0.0.
Deprecated since version NX9.0.0: Use overloaded function with enum instead.
License requirements: None.
-------------------------------------
Returns true if the characteristics builder contains all attributes with default values.
Signature
AreAttributesDefault(charxType)
Parameters: charxType ( NXOpen.Weld.CharacteristicsBuilderType
) – The type of characteristics being processedReturns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
ChangeFeatureType¶
-
CharacteristicsBuilder.
ChangeFeatureType
¶ Overloaded method ChangeFeatureType
ChangeFeatureType(weldType)
ChangeFeatureType(charxType)
-------------------------------------
Change the type of feature defining the attributes. Note after calling this method, the WeldJA::CharacteristicsValueBuilder objects previously retrieved will be invalid. You need to reaccess them if you want to make any changes to them.
Signature
ChangeFeatureType(weldType)
Parameters: weldType (int) – The type of welding feature being processed, see uf_weld_types.h. New in version NX7.5.0.
Deprecated since version NX9.0.0: Use overloaded function with enum instead.
License requirements: None.
-------------------------------------
Change the type of feature defining the attributes. Note after calling this method, the WeldJA::CharacteristicsValueBuilder objects previously retrieved will be invalid. You need to reaccess them if you want to make any changes to them.
Signature
ChangeFeatureType(charxType)
Parameters: charxType ( NXOpen.Weld.CharacteristicsBuilderType
) – The type of characteristics being processedNew in version NX9.0.0.
License requirements: None.
-------------------------------------
CopyAttributesFromObject¶
-
CharacteristicsBuilder.
CopyAttributesFromObject
¶ Copy the attributes that are on the object to the selection.
Signature
CopyAttributesFromObject(object)
Parameters: object ( NXOpen.NXObject
) – The object from which to copy the attributes.New in version NX8.0.0.
License requirements: None.
CopyAttributesFromObjectForPaint¶
-
CharacteristicsBuilder.
CopyAttributesFromObjectForPaint
¶ Copies the attributes that are on the object to the selection for paint.
Signature
CopyAttributesFromObjectForPaint(objectTag)
Parameters: objectTag ( NXOpen.NXObject
) – The object from which to copy the attributes.New in version NX10.0.0.
License requirements: None.
CopyNonActiveAttributesFromObject¶
-
CharacteristicsBuilder.
CopyNonActiveAttributesFromObject
¶ Copy the non active attributes that are on the object to the selection.
Signature
CopyNonActiveAttributesFromObject(object)
Parameters: object ( NXOpen.NXObject
) – The object from which to copy the attributes.New in version NX8.0.0.
License requirements: None.
CreateSelectionSet¶
-
CharacteristicsBuilder.
CreateSelectionSet
¶ Overloaded method CreateSelectionSet
CreateSelectionSet(weldType, data)
CreateSelectionSet(charxType, data)
-------------------------------------
Create a new selection set and add it to the list.
Signature
CreateSelectionSet(weldType, data)
Parameters: - weldType (int) – The type of welding feature being processed, see uf_weld_types.h.
- data (
NXOpen.NXObject
) – An object to retrieve the current attribute settings.
Returns: Return type: New in version NX7.5.0.
Deprecated since version NX9.0.0: Use overloaded function with enum instead.
License requirements: None.
-------------------------------------
Create a new selection set and add it to the list.
Signature
CreateSelectionSet(charxType, data)
Parameters: - charxType (
NXOpen.Weld.CharacteristicsBuilderType
) – The type of characteristics being processed - data (
NXOpen.NXObject
) – An object to retrieve the current attribute settings.
Returns: Return type: New in version NX9.0.0.
License requirements: None.
-------------------------------------
DoesObjectHaveAttributes¶
-
CharacteristicsBuilder.
DoesObjectHaveAttributes
¶ Copy the attributes that are on the object to the selection and returns a flag indicating whether the object actually has attributes.
Signature
DoesObjectHaveAttributes(object)
Parameters: object ( NXOpen.NXObject
) – The object from which to copy the attributes.Returns: Return type: bool New in version NX8.0.1.
License requirements: None.
HasActiveValues¶
-
CharacteristicsBuilder.
HasActiveValues
¶ Returns true if the characteristics builder has any active values.
Signature
HasActiveValues()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
InheritAttributesFromObject¶
-
CharacteristicsBuilder.
InheritAttributesFromObject
¶ Inherit the attributes that are on the object to the selection.
Signature
InheritAttributesFromObject(object)
Parameters: object ( NXOpen.NXObject
) – The object from which to inherit the attributes.New in version NX8.5.0.
License requirements: None.
RemoveAllAttributes¶
-
CharacteristicsBuilder.
RemoveAllAttributes
¶ Remove all attributes from the objects.
Signature
RemoveAllAttributes(objects)
Parameters: objects (list of NXOpen.NXObject
) – The objects to remove the attributes from.New in version NX8.0.0.
License requirements: None.
RemoveInheritedAttributes¶
-
CharacteristicsBuilder.
RemoveInheritedAttributes
¶ Remove any attributes that are inherited from other objects (for example, edges).
These will be attributes that are not required and are not in a category.
Signature
RemoveInheritedAttributes()
New in version NX8.0.1.
License requirements: None.
SetAllAttributesChanged¶
-
CharacteristicsBuilder.
SetAllAttributesChanged
¶ Overloaded method SetAllAttributesChanged
SetAllAttributesChanged()
SetAllAttributesChanged(status)
-------------------------------------
Sets all attributes to be changed.
Signature
SetAllAttributesChanged()
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Sets all attributes changed value to the status value.
Signature
SetAllAttributesChanged(status)
Parameters: status (bool) – The value to set changed value. true means attribute has been changed, false means attribute has not been changed New in version NX9.0.0.
License requirements: None.
-------------------------------------
Validate¶
-
CharacteristicsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.