UserDefinedWeldBuilder Class¶
-
class
NXOpen.Weld.
UserDefinedWeldBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Weld.UserDefinedWeldBuilder
builder.To create a new instance of this class, use
NXOpen.Weld.WeldManager.CreateUserDefinedWeldBuilder()
Default values.
Property Value AssignWeldPMI 0 New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AssignWeldPMI | Returns or sets the assign weld pmi. |
Characteristics | Returns the characteristics. |
Class4gd | Returns or sets the 4GD class option. |
SelectBody | Returns the select body. |
SelectConnectParts | Returns the select connect parts. |
SelectEdge | Returns the select edge. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
UserDefinedWeldBuilderWeldTypes Enumeration | Weld types for 4GD classes. |
Property Detail¶
AssignWeldPMI¶
-
UserDefinedWeldBuilder.
AssignWeldPMI
¶ Returns or sets the assign weld pmi.
-------------------------------------
Getter Method
Signature
AssignWeldPMI()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AssignWeldPMI(assignWeldPMI)
Parameters: assignWeldPMI (bool) – New in version NX7.5.0.
License requirements: ugweld (“UG WELD”)
Characteristics¶
-
UserDefinedWeldBuilder.
Characteristics
¶ Returns the characteristics.
-------------------------------------
Getter Method
Signature
Characteristics()
Returns: Return type: NXOpen.Weld.CharacteristicsBuilder
New in version NX7.5.0.
License requirements: None.
Class4gd¶
-
UserDefinedWeldBuilder.
Class4gd
¶ Returns or sets the 4GD class option.
-------------------------------------
Getter Method
Signature
Class4gd()
Returns: Return type: NXOpen.Weld.UserDefinedWeldBuilderWeldTypes
New in version NX10.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Class4gd(assignWeldPMI)
Parameters: assignWeldPMI ( NXOpen.Weld.UserDefinedWeldBuilderWeldTypes
) –New in version NX10.0.2.
License requirements: ugweld (“UG WELD”)
SelectBody¶
-
UserDefinedWeldBuilder.
SelectBody
¶ Returns the select body.
-------------------------------------
Getter Method
Signature
SelectBody()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX7.5.0.
License requirements: None.
SelectConnectParts¶
-
UserDefinedWeldBuilder.
SelectConnectParts
¶ Returns the select connect parts.
-------------------------------------
Getter Method
Signature
SelectConnectParts()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
SelectEdge¶
-
UserDefinedWeldBuilder.
SelectEdge
¶ Returns the select edge.
-------------------------------------
Getter Method
Signature
SelectEdge()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
UserDefinedWeldBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.