UserDefinedWeldBuilderWeldTypes Enumeration¶
NXOpen.Weld.UserDefinedWeldBuilder.WeldTypes is an alias for NXOpen.Weld.UserDefinedWeldBuilderWeldTypes
-
class
NXOpen.Weld.
UserDefinedWeldBuilderWeldTypes
¶ Bases:
object
Weld types for 4GD classes.
Enum Members
Enum Member Enum Member Description Groove Groove Weld type.Fillet Fillet Weld type.PlugSlot Plug Slot Weld type.Bead Bead Weld type.Fill Fill Weld type.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-