WeldCustom Enumeration

class NXOpen.Weld.WeldCustom

Bases: object

Settings for output solid type Enum Members

Enum Member Enum Member Description
SolidNone
creates only a point
SolidSphere
creates a sphere
SolidCylinder
creates a cylinder
SolidCone
creates a cone
SolidDefault
creates a default solid
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.