DatumCommonBuilderCustomTypes Enumeration¶
NXOpen.Weld.DatumCommonBuilder.CustomTypes is an alias for NXOpen.Weld.DatumCommonBuilderCustomTypes
-
class
NXOpen.Weld.
DatumCommonBuilderCustomTypes
¶ Bases:
object
The custom type of the datum specified for creation.
Enum Members
Enum Member Enum Member Description Default A datum surface or pin specified in the customer defaults by the Default type.Custom1 A datum surface or pin specified in the customer defaults by the Custom1 type.Custom2 A datum surface or pin specified in the customer defaults by the Custom2 type.Custom3 A datum surface or pin specified in the customer defaults by the Custom3 type.Custom4 A datum surface or pin specified in the customer defaults by the Custom4 type.Custom5 A datum surface or pin specified in the customer defaults by the Custom5 type.Custom6 A datum surface or pin specified in the customer defaults by the Custom6 type.Custom7 A datum surface or pin specified in the customer defaults by the Custom7 type.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-