WeldSelectionType Enumeration

class NXOpen.Weld.WeldSelectionType

Bases: object

the type of selction Enum Members

Enum Member Enum Member Description
General
general type
Surface
surface
Curve
curve
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.