WeldBeadBuilderOutputTypes Enumeration¶
NXOpen.Weld.WeldBeadBuilder.OutputTypes is an alias for NXOpen.Weld.WeldBeadBuilderOutputTypes
-
class
NXOpen.Weld.
WeldBeadBuilderOutputTypes
¶ Bases:
object
Settings to indicate the update behaviour of the bead feature
Enum Members
Enum Member Enum Member Description Fixed Bead does not recreate itself on update.Associative Bead follows normal update behaviour.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-