WeldJointBuilderApplication Enumeration¶
NXOpen.Weld.WeldJointBuilder.Application is an alias for NXOpen.Weld.WeldJointBuilderApplication
-
class
NXOpen.Weld.
WeldJointBuilderApplication
¶ Bases:
object
Application where joints are created.
Enum Members
Enum Member Enum Member Description StructureWelding Structure Welding Application.Routing Routing Application.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-