PlugSlotBuilder Class¶
-
class
NXOpen.Weld.
PlugSlotBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Weld.PlugSlot
builderTo create a new instance of this class, use
NXOpen.Weld.WeldManager.CreatePlugSlotBuilder()
Default values.
Property Value AssignWeldPMI 0 ContourDepth.Value 2.54 (millimeters part), .1 (inches part) ContourHeight.Value 2.54 (millimeters part), .1 (inches part) ContourType None FieldWeld 0 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AssignWeldPMI | Returns or sets the assign weld pmi |
Characteristics | Returns the characteristics |
ContourDepth | Returns the contour depth |
ContourHeight | Returns the contour height needed for cap |
ContourType | Returns or sets the contour type |
Edge1 | Returns the edge of the hole or slot on face1 |
Face1 | Returns the face1 |
Face2 | Returns the face2 |
FieldWeld | Returns or sets the field weld |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SeedFace1 | Returns or sets the top face on face1 |
SeedFace2 | Returns or sets the bottom face from which the weld will be extruded towards the top |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PlugSlotBuilderArcProcessEnum Enumeration | arc process for the weld feature |
PlugSlotBuilderEnumContour Enumeration | contour type |
Property Detail¶
AssignWeldPMI¶
-
PlugSlotBuilder.
AssignWeldPMI
¶ Returns or sets the assign weld pmi
-------------------------------------
Getter Method
Signature
AssignWeldPMI()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AssignWeldPMI(assignWeldPMI)
Parameters: assignWeldPMI (bool) – New in version NX8.0.0.
License requirements: None.
Characteristics¶
-
PlugSlotBuilder.
Characteristics
¶ Returns the characteristics
-------------------------------------
Getter Method
Signature
Characteristics()
Returns: Return type: NXOpen.Weld.CharacteristicsBuilder
New in version NX8.0.0.
License requirements: None.
ContourDepth¶
-
PlugSlotBuilder.
ContourDepth
¶ Returns the contour depth
-------------------------------------
Getter Method
Signature
ContourDepth()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
ContourHeight¶
-
PlugSlotBuilder.
ContourHeight
¶ Returns the contour height needed for cap
-------------------------------------
Getter Method
Signature
ContourHeight()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
ContourType¶
-
PlugSlotBuilder.
ContourType
¶ Returns or sets the contour type
-------------------------------------
Getter Method
Signature
ContourType()
Returns: Return type: NXOpen.Weld.PlugSlotBuilderEnumContour
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ContourType(contourType)
Parameters: contourType ( NXOpen.Weld.PlugSlotBuilderEnumContour
) –New in version NX8.0.0.
License requirements: None.
Edge1¶
-
PlugSlotBuilder.
Edge1
¶ Returns the edge of the hole or slot on face1
-------------------------------------
Getter Method
Signature
Edge1()
Returns: Return type: NXOpen.Section
New in version NX8.0.0.
License requirements: None.
Face1¶
-
PlugSlotBuilder.
Face1
¶ Returns the face1
-------------------------------------
Getter Method
Signature
Face1()
Returns: Return type: NXOpen.ScCollector
New in version NX8.0.0.
License requirements: None.
Face2¶
-
PlugSlotBuilder.
Face2
¶ Returns the face2
-------------------------------------
Getter Method
Signature
Face2()
Returns: Return type: NXOpen.ScCollector
New in version NX8.0.0.
License requirements: None.
FieldWeld¶
-
PlugSlotBuilder.
FieldWeld
¶ Returns or sets the field weld
-------------------------------------
Getter Method
Signature
FieldWeld()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FieldWeld(fieldWeld)
Parameters: fieldWeld (bool) – New in version NX8.0.0.
License requirements: None.
SeedFace1¶
-
PlugSlotBuilder.
SeedFace1
¶ Returns or sets the top face on face1
-------------------------------------
Getter Method
Signature
SeedFace1()
Returns: Return type: NXOpen.Face
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SeedFace1(seedFace1)
Parameters: seedFace1 ( NXOpen.Face
) –New in version NX8.0.0.
License requirements: None.
SeedFace2¶
-
PlugSlotBuilder.
SeedFace2
¶ Returns or sets the bottom face from which the weld will be extruded towards the top
-------------------------------------
Getter Method
Signature
SeedFace2()
Returns: Return type: NXOpen.Face
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SeedFace2(seedFace2)
Parameters: seedFace2 ( NXOpen.Face
) –New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
PlugSlotBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.