WeldJointBuilderDestinationTypes Enumeration

NXOpen.Weld.WeldJointBuilder.DestinationTypes is an alias for NXOpen.Weld.WeldJointBuilderDestinationTypes

class NXOpen.Weld.WeldJointBuilderDestinationTypes

Bases: object

Where to create new joints.

Enum Members

Enum Member Enum Member Description
WorkPart
Create new joints in work part.
NewComponent
Create a new componenent for each joint under the work part.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.