WeldAdvisorCheckerType Enumeration¶
-
class
NXOpen.Weld.
WeldAdvisorCheckerType
¶ Bases:
object
the type of checker Enum Members
Enum Member Enum Member Description CoincidentPoint Mimimum DistanceMinimumPointDistance minimum point distanceMinimumEdgeDistance minimum edge distanceStackUpGap stack up gapFacePlanarity face planarityFaceParallelism face parallelismPointFaceDistance point face distanceCsysFaceNormalAngle csys face normal angleMetalStackUp metal stack upMetalMinimumPointDatumDistance minimum point datum distanceMetalMinimumPointMeasurementDistance minimum point measurement distanceSpacingPerPanelCombination spacing per panel combinationWeldFlange weld flangeBead sealer beadNumber number of checkers-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-