JointmarkGuideBuilderLocation Enumeration

NXOpen.Weld.JointmarkGuideBuilder.Location is an alias for NXOpen.Weld.JointmarkGuideBuilderLocation

class NXOpen.Weld.JointmarkGuideBuilderLocation

Bases: object

The type of guide curve

Enum Members

Enum Member Enum Member Description
CenterLine
Centerline
OffsetFromEdge
Offset from Edge
ExistingCurve
Existing Curve
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.