AssociativeSplit |
Returns or sets whether split joints should be associative |
BackingFace |
Returns the backing face. |
BossColorFontWidth |
Returns the color, font, and width of the boss joint curves. |
ButtColor |
Returns or sets the color for butt weld type joints |
ButtColorFontWidth |
Returns the color, font, and width of the butt joint curves. |
ButtFont |
Returns or sets the curve font for butt weld type joints |
ButtWidth |
Returns or sets the curve with for butt weld type joints |
CombineConnectedJoints |
Returns or sets the indication to combine connected joints if they belong to the same body |
CornerColorFontWidth |
Returns the color, font, and width of the corner joint curves. |
CreateMethod |
Returns or sets the creation method |
CreatedApplication |
Returns or sets the application where joint is created |
Destination |
Returns or sets the destination to create new joints |
DuplicateCheck |
Returns or sets the indication to not allow new joints to be created if they are duplicates of exising joints |
FilletColor |
Returns or sets the color for T-joint weld type joints |
FilletFont |
Returns or sets the curve font for T-joint weld type joints |
FilletWidth |
Returns or sets the curve with for T-joint weld type joints |
Joint |
Returns the welding joint curves. |
JointList |
Returns the list of NXOpen.Weld.JointItemBuilder objects. |
JointPrefix |
Returns or sets the prefix for the weld ID attribute, and the prefix for the name of the component if NXOpen.Weld.WeldJointBuilderDestinationTypes is :py:class:` NXOpen.Weld.WeldJointBuilderDestinationTypes.NewComponent < NXOpen.Weld.WeldJointBuilderDestinationTypes>` |
LapColorFontWidth |
Returns the color, font, and width of the lap joint curves. |
LimitList |
Returns the list of limit builders. |
Limits |
Returns the limits of the joint curve span. |
MasterEdge |
Returns the master edge of a fillet weld. |
MaximumFaceGap |
Returns or sets the maximum face gap used when determining if two bodies intersect. |
MechanicalColorFontWidth |
Returns the color, font, and width of the mechanical joint curves. |
NamePrefix |
Returns or sets the prefix used for the welding joint Design Feature name in Collaborative Product Development mode |
NumberSegments |
Returns or sets the number of segments to divide a joint when using :py:class:` NXOpen.Weld.WeldJointBuilderSplitTypes.EqualSegments < NXOpen.Weld.WeldJointBuilderSplitTypes>`. |
PlacementFace |
Returns the placement face of a fillet weld. |
PrimaryEdge |
Returns the primary edge of a butt weld. |
PrimaryFace |
Returns the primary face of a butt weld. |
SecondaryEdge |
Returns the secondary edge of a butt weld. |
SecondaryFace |
Returns the secondary face of a butt weld. |
ShipComponent |
Returns the components on which the welding joints will be created. |
SleeveColorFontWidth |
Returns the color, font, and width of the sleeve joint curves. |
SocketColorFontWidth |
Returns the color, font, and width of the socket joint curves. |
SpacingLength |
Returns or sets the spacing length when using :py:class:` NXOpen.Weld.WeldJointBuilderSplitTypes.Skip < NXOpen.Weld.WeldJointBuilderSplitTypes>`. |
SplitAngle |
Returns or sets the split angle to divide a joint when using :py:class:` NXOpen.Weld.WeldJointBuilderSplitTypes.Angle < NXOpen.Weld.WeldJointBuilderSplitTypes>`. |
SplitLength |
Returns or sets the segment length when using :py:class:` NXOpen.Weld.WeldJointBuilderSplitTypes.Skip < NXOpen.Weld.WeldJointBuilderSplitTypes>`. |
SplitOption |
Returns or sets the method used to split the joint |
SubsetPart |
Returns or sets the subset part where Design Control Elements are to be created |
TJointColorFontWidth |
Returns the color, font, and width of the T-joint curves. |
Tag |
Returns the Tag for this object. |
TargetFace |
Returns the target face of a fillet weld. |
Type |
Returns or sets the creation type |
WeldType |
Returns or sets the weld type |
WeldingCharacteristics |
Returns the collection of welding characteristics defined by attributes. |
WorkPart |
Returns or sets the saved work part |