WeldJointBuilderWeldTypes Enumeration

NXOpen.Weld.WeldJointBuilder.WeldTypes is an alias for NXOpen.Weld.WeldJointBuilderWeldTypes

class NXOpen.Weld.WeldJointBuilderWeldTypes

Bases: object

Weld types.

Enum Members

Enum Member Enum Member Description
Any
Any Joint type.
Groove
Groove joint.
Fillet
T-Joint.
Corner
Corner joint.
Lap
Lap joint.
Socket
Socket joint for pipe welding.
Mechanical
Mechanical joint for pipe welding.
Sleeve
Sleeve joint for pipe welding.
Boss
Boss joint for pipe welding.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.